Error find my LVDS driver in imx8m mini Android OS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Error find my LVDS driver in imx8m mini Android OS

8,449 次查看
Ruban1
Contributor II

Error find my LVDS driver in imx8m mini Android OS

I have attached Log .

I have disabled the HDMI in my dts file and included LVDS

Even though I have disabled HDMI in Uboot its looking for HDMI only .How to config directly to get LVDS module.

i Hve attached the editted dts file also.

 

Kindly provide Solution

Thanks and regards

Ruban

 

 

标签 (1)
0 项奖励
回复
4 回复数

8,435 次查看
Ruban1
Contributor II

I am not able to understand . My question was very simple .. where should I equate the id=0x2c and instead of probing to default adv7535 which is HDMI. i want it to search and probe to sn65dsi83 which i have added the folder in kernel and .o file is also getting generated..in kernel everything going fine . My problem is uboot.. it not recognizing the driver, Its only searching of HDMI driver which is set as default somewhere ..I am not able to find that path. Can you kindly provide the path where i can edit to probe sn65dsi83 driver.

I have attached the screenshot below Error which i want to change the value I have made it bold

[*]-Video Link 0Can't find cec device id=0x3c
fail to probe panel device adv7535@3d
failed to get any video link display timings
probe video device failed, ret -22

[0] lcdif@32e00000, video
[1] mipi_dsi@32e10000, video_bridge
[2] adv7535@3d, panel
Can't find cec device id=0x3c
fail to probe panel device adv7535@3d
failed to get any video link display timings
probe video device failed, ret -22
In: serial
Out: serial
Err: serial

Thanks and regards

Ruban

0 项奖励
回复

8,164 次查看
Raghavendra
Contributor I

Hi Ruban,

Greetings...!!

Even I am also facing the same issue while integrating display in uboot.

could you please help me how did you fix this issue in uboot.

Thanks,

Raghavendra

 

0 项奖励
回复

8,429 次查看
igorpadykov
NXP Employee
NXP Employee

>My problem is uboot.. it not recognizing the driver, Its only searching
>of HDMI driver which is set as default somewhere

 

suggest to remove all adv7535 entries in dts, like :

&i2c2 {
clock-frequency = <400000>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_i2c2>;
scl-gpios = <&gpio5 18 GPIO_ACTIVE_HIGH>;
sda-gpios = <&gpio5 19 GPIO_ACTIVE_HIGH>;
status = "okay";

adv_bridge: adv7535@3d {
compatible = "adi,adv7533";
reg = <0x3d>;
adi,addr-cec = <0x3b>;
adi,dsi-lanes = <4>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_i2c2_synaptics_dsx_io>;
interrupt-parent = <&gpio1>;
interrupts = <9 IRQ_TYPE_LEVEL_LOW>;
status = "disabled"; /* changed from okay to disable */

port {
adv7535_from_dsim: endpoint {
remote-endpoint = <&dsim_to_adv7535>;
};
};
};..

 

 

0 项奖励
回复