Error during debug of Motor control software in MIMXRT1060

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error during debug of Motor control software in MIMXRT1060

905 Views
AnweshaPanda
NXP Employee
NXP Employee

I downloaded the latest motor control software example from SDK store. I can build it but it encounters error bus fault ( while debug. See picture. Please suggest a solution. 

AnweshaPanda_0-1631002409171.png

 

AnweshaPanda_0-1631003262086.png

 

 

0 Kudos
Reply
1 Reply

891 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello AnweshaPanda,

The mc_pmsm example requires some hardware setup, which can be found on the Application User’s Guide which is mentioned on the example readme under the doc folder.

The user guide does include the hardware setup for the i.MXRT1060-EVK, which includes some jumper settings and placing some resistors on the bottom side of the board. I would start by double checking that all the hardware is setup correctly.

Regards,
Gustavo

0 Kudos
Reply