Error building yocto project image

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error building yocto project image

ソリューションへジャンプ
3,016件の閲覧回数
waynetsui
Contributor II

BSP: imx-3.14.28-1.0.0_ga

0 件の賞賛
返信
1 解決策
1,841件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Wayne Tsui,

It is most likely that the problem resides in that you’re using the FSL BSP Release and not the FSL Community BSP. The former does not support the RioTboard and that’s why the image cannot be built for that target.

Please download the FSL Community BSP and try baking the image for the RioTboard with it. There is information on where to download it on the following link:

FSL Community BSP

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,841件の閲覧回数
waynetsui
Contributor II

$ MACHINE=imx6dl-riotboard  source fsl-setup-release.sh -b RIoTboard -e fb

$ bitbake  -k core-image-minimal

ERROR: Function failed: do_compile (log file is located at /home/wayne/yocto/fsl-release-bsp/RIoTboard-build/tmp/work/imx6dl_riotboard-poky-linux-gnueabi/u-boot-imx/2014.04-r0/temp/log.do_compile.29021)

ERROR: Logfile of failure stored in: /home/wayne/yocto/fsl-release-bsp/RIoTboard-build/tmp/work/imx6dl_riotboard-poky-linux-gnueabi/u-boot-imx/2014.04-r0/temp/log.do_compile.29021

Log data follows:

| DEBUG: Executing shell function do_compile

| NOTE: make -j 3 CROSS_COMPILE=arm-poky-linux-gnueabi- CC=arm-poky-linux-gnueabi-gcc  --sysroot=/home/wayne/yocto/fsl-release-bsp/RIoTboard-build/tmp/sysroots/imx6dl-riotboard riotboard_defconfig

| make: *** No rule to make target `riotboard_defconfig'.  Stop.

| ERROR: oe_runmake failed

| WARNING: exit code 1 from a shell command.

| ERROR: Function failed: do_compile (log file is located at /home/wayne/yocto/fsl-release-bsp/RIoTboard-build/tmp/work/imx6dl_riotboard-poky-linux-gnueabi/u-boot-imx/2014.04-r0/temp/log.do_compile.29021)

ERROR: Task 238 (/home/wayne/yocto/fsl-release-bsp/sources/meta-fsl-bsp-release/imx/meta-fsl-arm/recipes-bsp/u-boot/u-boot-imx_2014.04.bb, do_compile) failed with exit code '1'

WARNING: QA Issue: pulseaudio-module-console-kit rdepends on consolekit, but it isn't a build dependency? [build-deps]

Currently 1 running tasks (2008 of 2036):

0: linux-imx-3.14.28-r0 do_fetch (pid 15820)

0 件の賞賛
返信
1,842件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Wayne Tsui,

It is most likely that the problem resides in that you’re using the FSL BSP Release and not the FSL Community BSP. The former does not support the RioTboard and that’s why the image cannot be built for that target.

Please download the FSL Community BSP and try baking the image for the RioTboard with it. There is information on where to download it on the following link:

FSL Community BSP

0 件の賞賛
返信
1,841件の閲覧回数
waynetsui
Contributor II

Thank you , gusarambula.

0 件の賞賛
返信