Error build Linux 2.6.35 kernel with minicom

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Error build Linux 2.6.35 kernel with minicom

2,917 次查看
JayWilliamStubb
Contributor II

Hi All,

  I wanted to include minicom in my kernel to assist me in debugging my Host USB Serial port on the i.MX28 EVK. I have Linux 2.6.35 installed. I first ran into problems after selecting minicom in LTIB and trying to build the kernel. Minicom wasn't found. I was able to get Tech Support to send me the missing file (minicom_2.2.orig.tar.gz), but when I build the kernel, I get errors (window.h:154: error: conflicting types for 'wprintf'). See the attached file for a complete screen dump.

  Any ideas on how to get this to build correctly? Is there a patch?

  Is there a later version that works or an alternative that will do the same things?

标记 (2)
3 回复数

2,425 次查看
kurt1z
Contributor I

Thanks James,

for the solution, I have had the same problem on the imx53qsb board.

gr.

Kurt

James Robinson said:

I am running LTIB for the iMX28EVK, I did an upgrade to the minicom to compile the 2.6.1 version, and it compiled fine.

To do this, edit the dist/lfs-5.1/minicom/minicom.spec and replace the Version with 2.6.1 from 2.2 Also replace the version in the URL field..

You can get the source from:

http://ftp.debian.org/debian/pool/main/m/minicom

It is at the bottom of the listings. Copy it into the /opt/freescale/pkgs and rebuild with ./ltib

Hope it helps.....

James

0 项奖励
回复

2,425 次查看
JamesRobinson
Contributor II

I am running LTIB for the iMX28EVK, I did an upgrade to the minicom to compile the 2.6.1 version, and it compiled fine.

To do this, edit the dist/lfs-5.1/minicom/minicom.spec and replace the Version with 2.6.1 from 2.2 Also replace the version in the URL field..

You can get the source from:

http://ftp.debian.org/debian/pool/main/m/minicom

It is at the bottom of the listings. Copy it into the /opt/freescale/pkgs and rebuild with ./ltib

Hope it helps.....

James

2,425 次查看
enaud
Contributor III

Also me have this error!!!!

0 项奖励
回复