Hello everybody,
I'm tryng to debug my Linux OS for a custom iMX93 board. I'm able to start the OS but sometimes I get the following error while booting:
  
the weird fact is that this happens randomly! Sometimes I don't have problems at all, other times it hangs with this error and in different "locations" of the log! I understand that this error means that it cannot initialize a driver, comparing the error log with the correct one I'm able to discover which driver is not working. I'm wondering if could be a problem linked to the RAM settings. In particular when the OS starts, I notice that the RAM memory is not correctly recognized by the kernel (2 GB while I have only 256 MB):
 
Can anyone help me to understand what's going on?
Regards,
Bob
Hello,
The "Unable to handle kernel paging request at virtual address" error, often accompanied by a kernel panic, typically indicates a problem with memory access or mapping during kernel operations. This error can be caused by issues with device drivers, incorrect RAM settings, or even kernel bugs.
Hello,
Regarding the troubleshooting steps:
1. the virtual address changes! Everytime I reboot the board, and the problem occurs, the virtual address is never the same (when it doesn't work, because sometimes the kernel works!).
2. I didn't update any driver, I used the kernel version provided by NXP 6.12.y. I'm currently disabling all the drivers that I don't need in the menuconfig.
3. I set a bootarg ( mem=256M) in U-boot environment to let the kernel recognize the RAM size, otherwise it set 2GB by default. I don't know if it is the right way, please tell me.
5. The error changes.
6. Please, can you tell me how it has to be?
7,8 need to be examined.
Thanks in advance.
Regards,
Bob
Hello,
A1. Erase yocto and restart building again.
A2, try to check the CMEM variable in uboot.
Regards
Hello @Bio_TICFSL ,
Already done various builds, I still get the same random problem. Furthermore I didn't find the cmem variable.
Do you have any other suggestion regarding the possible cause of this weird behavior?
Regards,
Bob