Error: MCUXpresso SDK import failed. Selected file/folder is not a valid GCC ARM Embedded SDK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error: MCUXpresso SDK import failed. Selected file/folder is not a valid GCC ARM Embedded SDK

1,482件の閲覧回数
Jayadev
Contributor I

Hi I tried importing repository for i.MX RT1064 Evaluation Kit. I am using SDK_2_14_0_EVK-MIMXRT1064.zip . While importing the zip file in VSCode "Error: MCUXpresso SDK import failed. Selected file/folder is not a valid GCC ARM Embedded SDK". In the current supported devices in the MCUXpresso for Visual Studio Code webpage, Software details section > Supported Devices, I checked 

  • i.MX-RT1064 is present.

    I have installed required softwares using MCUXpresso Installer.
    Can you help me with this?
0 件の賞賛
返信
2 返答(返信)

1,385件の閲覧回数
Jayadev
Contributor I

Hi @RaRo 

Thank you for your reply. My host system is Ubuntu. So I installed MCU Xpresso IDE and tried to build example application. It was successful. Thank you for your help.

0 件の賞賛
返信

1,463件の閲覧回数
RaRo
NXP TechSupport
NXP TechSupport

Hello @Jayadev,

Just for double check, could you please check that the SDK you are trying to import/add to VS Code is for ARM GCC/MCUXpresso for VS Code instead of MCUXpresso IDE?

You could download the ARM GCC/MCUXpresso for VS Code SDK here. In the Build SDK section choose Toolchain/IDE as ARM GCC/MCUxpresso for VS Code before clicking on Download SDK.

RaRo_0-1702050678614.png

[Build SDK for EVK-MIMXRT1064]

Warm regards, Raul.

0 件の賞賛
返信