Error Building Process Stopped in imx8mm
i added GPIO in imx8mm-evk.dts file inside freescale folder
&iomuxc {
pinctrl-0 = <&pinctrl_hog_1>;
pinctrl_hog_1: hoggrp-1 {
fsl,pins = <
MX8MM_IOMUXC_GPIO1_IO08_GPIO1_IO8 0x19
MX8MM_IOMUXC_SAI5_RXD3_GPIO3_IO24 0x41
>;
};
};
Wen i run ./imx-make.sh
It stops inbetween i hve attached a screenshot.
You may take this for reference.
&iomuxc {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_hog>;
pinctrl_hog: hoggrp {
fsl,pins = <
IMX8QXP_MCLK_OUT0_ADMA_ACM_MCLK_OUT0 0x0600004c
IMX8QXP_COMP_CTL_GPIO_1V8_3V3_GPIORHB_PAD 0x000514a0
>;
};
imx8mm.dtsi is for the chip. You should modify the dts or dtsi file for the board. There should have a imx8mm-evk.dts for the evk board.
i have imx8mm-evk.dts file
in that i hve & iomux but inside that function. imx8mm-evk function is not available .
I have attached the file below
So to add
MX8MM_IOMUXC_SAI5_RXD3_GPIO3_IO24 0x41
In which inner function should i add .So it wil be available in below path
$ ls /sys/class/gpio
So, I shown you the example in imx8x-mek.dtsi above. You can do the same in imx8mm-evk.dts.