Errata workaround implementation status by i.MX6 android BSP.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Errata workaround implementation status by i.MX6 android BSP.

ソリューションへジャンプ
2,042件の閲覧回数
satoshishimoda
Senior Contributor I

Hi community,

I want to confirm the errata workaround implementation status by android BSP.

Please see ERR006233 in IMX6DQCE Rev.3.

It says "Implemented in BSP version Post GA L3.0.35_1.1.0".

I think android BSP (jb4.2.2_1.0.0-ga) also implemented the workaround because it uses same linux kernel as linux BSP.

Is this correct?

And how about other errata?

ALL workaround implementation status for android BSP is same as Linux BSP?

Best Regards,

Satoshi Shimoda

ラベル(3)
タグ(1)
0 件の賞賛
返信
1 解決策
1,590件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

You are correct the Android BSP  of Jellybean 4.2.2 uses the kernel L3.0.35_1.1.0, so if you review the Linux Release Notes document you can find which defects has been solved and which errata has been patch.  Or the other option it is to review the Errata document of the device which mentions which ones have a workaround by software.


Have a great day,
Jaime

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,590件の閲覧回数
satoshishimoda
Senior Contributor I

Somebody can reply?

0 件の賞賛
返信
1,591件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

You are correct the Android BSP  of Jellybean 4.2.2 uses the kernel L3.0.35_1.1.0, so if you review the Linux Release Notes document you can find which defects has been solved and which errata has been patch.  Or the other option it is to review the Errata document of the device which mentions which ones have a workaround by software.


Have a great day,
Jaime

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信