Errata workaround implementation status by i.MX6 android BSP.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Errata workaround implementation status by i.MX6 android BSP.

Jump to solution
2,082 Views
satoshishimoda
Senior Contributor I

Hi community,

I want to confirm the errata workaround implementation status by android BSP.

Please see ERR006233 in IMX6DQCE Rev.3.

It says "Implemented in BSP version Post GA L3.0.35_1.1.0".

I think android BSP (jb4.2.2_1.0.0-ga) also implemented the workaround because it uses same linux kernel as linux BSP.

Is this correct?

And how about other errata?

ALL workaround implementation status for android BSP is same as Linux BSP?

Best Regards,

Satoshi Shimoda

Labels (3)
Tags (1)
0 Kudos
Reply
1 Solution
1,630 Views
jamesbone
NXP TechSupport
NXP TechSupport

You are correct the Android BSP  of Jellybean 4.2.2 uses the kernel L3.0.35_1.1.0, so if you review the Linux Release Notes document you can find which defects has been solved and which errata has been patch.  Or the other option it is to review the Errata document of the device which mentions which ones have a workaround by software.


Have a great day,
Jaime

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
1,630 Views
satoshishimoda
Senior Contributor I

Somebody can reply?

0 Kudos
Reply
1,631 Views
jamesbone
NXP TechSupport
NXP TechSupport

You are correct the Android BSP  of Jellybean 4.2.2 uses the kernel L3.0.35_1.1.0, so if you review the Linux Release Notes document you can find which defects has been solved and which errata has been patch.  Or the other option it is to review the Errata document of the device which mentions which ones have a workaround by software.


Have a great day,
Jaime

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply