Encrypted storage using CAAM on linux-imx v5.4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Encrypted storage using CAAM on linux-imx v5.4

2,733 Views
fahad_arslan
Contributor II

Following app note is based on linux-imx v4.14 and has patches applicable to kernel v4.14.

https://www.nxp.com/docs/en/application-note/AN12714.pdf 

How can storage encryption using CAAM be done using linux-imx v5.4?

Thanks,

Fahad

3 Replies

2,640 Views
Yuri
NXP Employee
NXP Employee

Hello,

  I've sent You directly some comments.

Regards,

Yuri.

0 Kudos
Reply

2,532 Views
kile964
Contributor II

Hello Yuri,

Can you share this information with me as well?

0 Kudos
Reply

2,634 Views
aleksandar_niko
Contributor III

Hello Yuri,

could you share the same info with me as I am also working on the same thing (rootfs encryption with 5.4 Linux from initramfs).

Best,

Aleksandar

0 Kudos
Reply