Encrypted firmware via JTAG

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Encrypted firmware via JTAG

420 次查看
giuseppescarpi
Contributor III

Hi Yuri,

as Luis, we need to work with encrypted images, in two modes:

1) first programming (load image to QSPI, burn fuses/keys etc.)

2) on-the-fied upgrade (new firmware received via ETH).

According to your comment, we need USB or UART1 and the MFG tool.

On the other hand, the comment is four months old, so I would like to check.

Can you confirm that we cannot write an encrypted image via JTAG?

What if we just want a SIGNED image?

Moreover, what is the best method to execute the on-the-field upgrade?

Thanks

Giuseppe

0 项奖励
1 回复

368 次查看
Yuri
NXP Employee
NXP Employee

Hello,

   Generally both methods (MFG / USB and JTAG)  may be applied to update

secure (signed or encrypted) firmware. For MFG the signed flashloader should

be applied; for JTAG secure mode of JTAG must be used.  


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励