Encrypted boot on i.MX 6UL not working

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Encrypted boot on i.MX 6UL not working

1,395件の閲覧回数
kanimozhi_t
Contributor V

We tried encrypted boot on i.MX 6UL EVK with the AN12056 reference. We tried both procedures,

   1. Signing and encrypting the signed image 

   2. Encrypting and signing the encrypted image

In both cases the board is not booting and we're not even able to debug anything. Here is the list of commands we've followed,

hexdump -e '/4 "%X""\n"' -s 20 -n 4 u-boot-dtb.imx
hexdump u-boot-dtb.imx | tail -n 1
~/Downloads/cst-3.3.0/linux64/bin/cst -o csf_enc.bin -i u-boot_enc.csf
cp u-boot-dtb.imx u-boot-dtb.imx.dummy
~/Downloads/cst-3.3.0/linux64/bin/cst -o csf_sign_enc.bin -i u-boot_sign_enc.csf
du -b csf_enc.bin
# Nonce/MAC = 2248 - 36
dd if=csf_enc.bin of=noncemac.bin bs=1 skip=2212 count=36
dd if=noncemac.bin of=csf_sign_enc.bin bs=1 seek=2212 count=36
objcopy -I binary -O binary --pad-to 0x2000 --gap-fill=0xff csf_sign_enc.bin csf_sign_enc_padded.bin
# signed and unencrypted U-Boot
cat u-boot-dtb.imx csf_sign_enc_padded.bin > u-boot_encrypted_no_dek.bin
sudo dd if=u-boot_encrypted_no_dek.bin of=/dev/sdc bs=1K seek=1 && sync

Hereby I've attached the following,

   1. CSF for encryption

   2. CSF signing the encrypted u-boot

Any help on this regard would be highly appreciated.

ラベル(2)
タグ(2)
0 件の賞賛
返信
2 返答(返信)

1,279件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Kanimozhi

I sent additional materials via mail.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,280件の閲覧回数
kanimozhi_t
Contributor V

Thanks igorpadykov‌ The issue has been resolved now!

0 件の賞賛
返信