How can I enable ecspi4 on iMX6ULL 14x14 evk?
I enabled IMX_SPI feature in menuconfig and add below in device tree file
&ecspi4 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_ecspi4>;
num-chipselects = <1>;
status = "okay";
};
But, kernel log shows below error
spi_imx: probe of 2014000.ecspi failed with error -22
Please help me to enable ecspi4 in the evk.
Solved! Go to Solution.
Self Answer.
num-chipselects = <1>;
is not correct. this should be
fsl,spi-num-chipselects = <1>;
Let me sum-up to enable ECSPI4 in iMX6ULL-14x14 evk.
In file imx6ull-14x14-evk.dts, add below
&ecspi4 {
fsl,spi-num-chipselects = <1>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_ecspi4>;
status = "okay";
};
And add below in &iomuxc node
pinctrl_ecspi4: ecspi4grp {
fsl,pins = <
MX6UL_PAD_ENET2_TX_CLK__ECSPI4_MISO 0x4001b031
MX6UL_PAD_ENET2_TX_EN__ECSPI4_MOSI 0x1b0b0
MX6UL_PAD_ENET2_TX_DATA1__ECSPI4_SCLK 0x1b0b0
MX6UL_PAD_ENET2_RX_ER__ECSPI4_SS0 0x1b0b0
>;
};
Best Regards
Self Answer.
num-chipselects = <1>;
is not correct. this should be
fsl,spi-num-chipselects = <1>;
Let me sum-up to enable ECSPI4 in iMX6ULL-14x14 evk.
In file imx6ull-14x14-evk.dts, add below
&ecspi4 {
fsl,spi-num-chipselects = <1>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_ecspi4>;
status = "okay";
};
And add below in &iomuxc node
pinctrl_ecspi4: ecspi4grp {
fsl,pins = <
MX6UL_PAD_ENET2_TX_CLK__ECSPI4_MISO 0x4001b031
MX6UL_PAD_ENET2_TX_EN__ECSPI4_MOSI 0x1b0b0
MX6UL_PAD_ENET2_TX_DATA1__ECSPI4_SCLK 0x1b0b0
MX6UL_PAD_ENET2_RX_ER__ECSPI4_SS0 0x1b0b0
>;
};
Best Regards
Hi Mannsik,
you need also to enable the pins in the iomux node on dts.
You can see next document for reference.
Basic Device Tree for the Udoo Board
And the post below explains what the parameters on this node are:
32Khz clock on CCM_CLKO2 (SD1_WP)
Best regards,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
I added below in iomuxc node, but result is same as before.
pinctrl_ecspi4: ecspi4grp {
fsl,pins = <
MX6UL_PAD_ENET2_TX_CLK__ECSPI4_MISO 0x70a1
MX6UL_PAD_ENET2_TX_EN__ECSPI4_MOSI 0x70a1
MX6UL_PAD_ENET2_TX_DATA1__ECSPI4_SCLK 0x70a1
MX6UL_PAD_ENET2_RX_ER__ECSPI4_SS0 0x70a1
>;
};
Please, let me know what I'm missing.