Hello,
I have a wifi module (Marvel 8797 - SDIO 3.0) that is connected to USDHC4.
My pinmux settings for my port as follow: (LVE is enabled).
CLK 0x4170b9
CMD 0x4170b9
DAT0 0x4170b9
DAT1 0x4170b9
DAT2 0x4170b9
DAT3 0x4170b9
My wifi module works on 1-bit mode but not on 4-bit mode. That is because the SDIO 3.0 require an UHSI (it require 1.8v signaling) enabled and by default, the kernel seems not configured for the said mode.
I would like to know what are the missing keys in order to enable it correctly?.
Regards,
john
已解决! 转到解答。
Yes.
VSELECT is an output signal used to change the voltage of the external power supplier.
See bit definition in imx6q/dl spec:
For details you can refer to imx6q/dl reference mannual.
BTW, imx6q sabresd does not have a external control circuit on board to switch signal voltage between 1.8v and 3.3v.
That means imx6q sabresd does not support working on 1.8v mode, as a result, not support SDIO3.0 too.
If you want to try SDIO3.0 you can use imx6q/dl sabreauto board which has that external voltage control circuit on board or imx6sl evk.
Regards
Dong Aisheng
Hello,
Follow up to my previous post. In freescale linux kernel 3.5.7 alpha release, the device tree for iMX6q-sabresd, the USDHC3 pinctrl settings has SD3_VSELECT. Can anyone could give me some information what exactly the purpose of the said pin?. Is that pin is being use for voltage signaling for UHS-I?.
Regards,
john
Yes.
VSELECT is an output signal used to change the voltage of the external power supplier.
See bit definition in imx6q/dl spec:
For details you can refer to imx6q/dl reference mannual.
BTW, imx6q sabresd does not have a external control circuit on board to switch signal voltage between 1.8v and 3.3v.
That means imx6q sabresd does not support working on 1.8v mode, as a result, not support SDIO3.0 too.
If you want to try SDIO3.0 you can use imx6q/dl sabreauto board which has that external voltage control circuit on board or imx6sl evk.
Regards
Dong Aisheng
Hi Dong,
In i.MX6SL there are 2 power domains for GPIO. These are NVCC33_IO and NVCC18_IO. And there is no dedicated pin for SD interface. So which domain is supposed to be controlled by VSELECT bit/pin? Is it for controlling the power supply for SD cards to support different type of cards. And I am assuming that the IO voltage for SDIO interface pads will be automatically taken care by i.MX6SL based on VSELECT bit.
Is my understanding correct?
Regards,
Vinod