Enabling Power on Self Test (POST) IMx6solox

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Enabling Power on Self Test (POST) IMx6solox

2,193件の閲覧回数
niranjanbc
Contributor IV

Hi

I am looking to enable the "POST" (POST_CONFIG) in U-boot running on IMX6SoloX, to enable that i need non volatile memory address for _POST_WORD_ADDR. do we have any solution for that. can use the NOR flash address i have my board or it should be onchip memory only.

THANKS

Niranjan

ラベル(3)
2 返答(返信)

1,711件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Niranjan

I am afraid "POST" is not supported in nxp uboot releases and
this may be posted on uboot mail list
https://lists.denx.de/listinfo/u-boot

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,711件の閲覧回数
niranjanbc
Contributor IV

Thanks for the response Igor,

we are looking for some thing like POST to do bare minimal test on power up.

if POST is not supported do we have any other option for self test.

For 1 Gbyte DDR ram test i see there is a mtest, but which is very slow. 

thanks

Niranjan

0 件の賞賛
返信