Enabling LCD display in i.MX50 EVK with Linux release -blog archive

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Enabling LCD display in i.MX50 EVK with Linux release -blog archive

1,182 次查看
GraceH
Senior Contributor II

In Linux BSP, by default, the LCD framebuffer is not enabled.  SEIKO and CLAA driver are also disabled.

The kernel need be re-configure to enable LCD framebuffer.

In kernel configuration menu, go to device drivers -> Graphics Support

Select "SEIKO WVGA Panel"

Select "CLAA WVGA Panel"

Deselect "E-ink Panel Framebuffer"

Select "Support MXC ELCDIF framebuffer"

Then in command line:

 

1. with SEIKO LCD (connected on J13)

setenv bootargs_mmc 'setenv bootargs ${bootargs} console=ttymxc0 root=/dev/mmcblk0p2 rootwait rw lcd=1'

2. with SEIKO LCD (connected on J12)

setenv bootargs_mmc 'setenv bootargs ${bootargs} console=ttymxc0 root=/dev/mmcblk0p2 rootwait rw lcd=1,j12'

2. with CLAA LCD

setenv bootargs_mmc 'setenv bootargs ${bootargs} console=ttymxc0 root=/dev/mmcblk0p2 rootwait rw lcd=2'

标记 (1)
0 项奖励
回复
0 回复数