Enabling GNSS on iMX8 QM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Enabling GNSS on iMX8 QM

416件の閲覧回数
swayamdhondge10
Contributor II

I want to know how we can connect a GNSS receiver to the imx8 qm baord as it doesn't support in-built gnss module. Would appreciate if someone can guide me to a detailed document on this.

Also, how I can connect to a CAN signal generator.


ラベル(1)
0 件の賞賛
返信
3 返答(返信)

380件の閲覧回数
swayamdhondge10
Contributor II

Thanks for the reply.
Is there any plug and play module or chip available which can be plugged to the NXP iMX8 qm and used as a GNSS receiver. 

0 件の賞賛
返信

362件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

no official suggestion module which can plug to the imx8qm directly, but imx8qm has M.2 port, if the GNSS module support M.2 connector, maybe you can try it, suggest that you can refer to the 8qm schematic firstly 

0 件の賞賛
返信

404件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

don't find such specific solution for GNSS on imx8qm, you can refer to the can settings, then add by yourself

https://github.com/nxp-imx/linux-imx/blob/lf-6.12.y/arch/arm64/boot/dts/freescale/imx8qm-mek.dts

you also can refer to another customer who enable this with uart

https://community.nxp.com/t5/i-MX-Processors/How-do-we-use-iMX8QM-s-uart-to-recieve-GNSS-module-data...

 

0 件の賞賛
返信