Enable wifi bluetooth and GPIO from boot Yocto i.MX 8M plus

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Enable wifi bluetooth and GPIO from boot Yocto i.MX 8M plus

ソリューションへジャンプ
1,238件の閲覧回数
dvega
Contributor II

I build the imx-image-full. I was able to get the wifi, and bluetooth up and running by executing the commands described here https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/How-to-use-Bluetooth-on-i-MX8M-boards/ta...

What I want now is to enable them from yocto. Meaning when the image is build. Once you flash it. then it will already have the wifi and bluetooth and GPIO up and ready to go. I'm not sure on how to convert/create/append a recipe to enable all of that.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,203件の閲覧回数
brian14
NXP TechSupport
NXP TechSupport

Hi @dvega

Thank you for contacting NXP Support.

For WIFI and Bluetooth you can try using a service similar to the service described on the following community article:
Enable WIFI on Ubuntu 22.04 and Linux BSPs in iMX8 Family - NXP Community

I hope this information will be helpful.

Have a great day!

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,204件の閲覧回数
brian14
NXP TechSupport
NXP TechSupport

Hi @dvega

Thank you for contacting NXP Support.

For WIFI and Bluetooth you can try using a service similar to the service described on the following community article:
Enable WIFI on Ubuntu 22.04 and Linux BSPs in iMX8 Family - NXP Community

I hope this information will be helpful.

Have a great day!

0 件の賞賛
返信