Enable wifi bluetooth and GPIO from boot Yocto i.MX 8M plus

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Enable wifi bluetooth and GPIO from boot Yocto i.MX 8M plus

Jump to solution
592 Views
dvega
Contributor II

I build the imx-image-full. I was able to get the wifi, and bluetooth up and running by executing the commands described here https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/How-to-use-Bluetooth-on-i-MX8M-boards/ta...

What I want now is to enable them from yocto. Meaning when the image is build. Once you flash it. then it will already have the wifi and bluetooth and GPIO up and ready to go. I'm not sure on how to convert/create/append a recipe to enable all of that.

0 Kudos
Reply
1 Solution
557 Views
brian14
NXP TechSupport
NXP TechSupport

Hi @dvega

Thank you for contacting NXP Support.

For WIFI and Bluetooth you can try using a service similar to the service described on the following community article:
Enable WIFI on Ubuntu 22.04 and Linux BSPs in iMX8 Family - NXP Community

I hope this information will be helpful.

Have a great day!

View solution in original post

0 Kudos
Reply
1 Reply
558 Views
brian14
NXP TechSupport
NXP TechSupport

Hi @dvega

Thank you for contacting NXP Support.

For WIFI and Bluetooth you can try using a service similar to the service described on the following community article:
Enable WIFI on Ubuntu 22.04 and Linux BSPs in iMX8 Family - NXP Community

I hope this information will be helpful.

Have a great day!

0 Kudos
Reply