Enable pstore(ramoops) on i.MX8MM - changes in Kernel Configs and DTS not working

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Enable pstore(ramoops) on i.MX8MM - changes in Kernel Configs and DTS not working

940 Views
harsh1621
Contributor II

I'm looking to have persistent kernel logs across reboots in case of a Kernel Panic. I looked up to find that pstore (ramoops) can be used to achieve the same. However, I'm unable to get any logs across reboots when a kernel panic occurs.

Following are the changes that I've done:

Kernel (4.19.35) Configs:

CONFIG_PSTORE=y
CONFIG_PSTORE_DEFLATE_COMPRESS=y
CONFIG_PSTORE_COMPRESS=y
CONFIG_PSTORE_DEFLATE_COMPRESS_DEFAULT=y
CONFIG_PSTORE_COMPRESS_DEFAULT="deflate"
CONFIG_PSTORE_CONSOLE=y
CONFIG_PSTORE_RAM=y

DTS Changes:

reserved-memory {
        #address-cells = <2>;
        #size-cells = <2>;
        ranges;

        ramoops: ramoops@ffdfffff {
        compatible = "ramoops";
        reg = <0 0xffdfffff 0 0x100000>;
        record-size = <0x20000>;
        console-size = <0x20000>;
        ftrace-size = <0x20000>;
    };

Following are the dmesg logs corresponding to ramoops and pstore:

[ 2.031079] pstore: Registered ramoops as persistent store backend
[ 2.043195] ramoops: attached 0x100000@0xffdfffff, ecc: 0/0

[ 1.005114] pstore: using deflate compression
[ 2.027306] console [pstore-1] enabled
[ 2.031079] pstore: Registered ramoops as persistent store backend

Using the following to trigger a reboot on kernel panic:

echo 10 > /proc/sys/kernel/panc

echo c > /proc/sysrq-trigger

**** Kernel Panic starts and system reboots after 10 secs ****

On reboot, the /sys/fs/pstore directory is empty and no logs are found.

What am I missing in the above? Do I need to use different RAM addresses? Or is persistent storage using ramoops even supported on the (Variscite) iMX8MM boards?

 

Tags (3)
0 Kudos
Reply
0 Replies