Enable kernel configuration options like CONFIG_PROFILING and CONFIG_PERF_EVENTS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Enable kernel configuration options like CONFIG_PROFILING and CONFIG_PERF_EVENTS

2,430 次查看
mohamad-ahmad
Contributor III

Hello,

Can someone help me how I can change the kernel configurations by enabling certain of them like CONFIG_PERF_EVENTS and CONFIG_PROFILING.

Normally when I check some configurations I find, for example:

# XXXXXX is not set

or

YYYYYY=y

Thank you for the help

标签 (1)
0 项奖励
回复
2 回复数

1,858 次查看
mohamad-ahmad
Contributor III

thank you Yuri.

Mohamad

0 项奖励
回复

1,857 次查看
Yuri
NXP Employee
NXP Employee

Hello,

The following may be useful :

Task #5 - Kernel

i.MX Yocto Project: How can I patch the kernel?

i.MX Yocto Project: How can I compile the kernel manually?

i.MX Yocto Project: Frequently Asked Questions

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复