Enable ethernet Wake-On-LAN feature on i.MX8 with Android

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Enable ethernet Wake-On-LAN feature on i.MX8 with Android

3,186件の閲覧回数
yyc1975
Contributor III

Hi All,

We can enable WoL feature on Yocto linux and wakeup device from suspend.

It fails to wakeup system when change to Android.

Did anyone knows how to enable WoL feature on Android OS?

Best Regards,

YY

0 件の賞賛
返信
5 返答(返信)

3,089件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Which android BSP are you using?

0 件の賞賛
返信

3,089件の閲覧回数
yyc1975
Contributor III

Hi b45499,

We are using Android P9.0.0_2.3.2 (Linux 4.14 kernel) Android P9.0.0_2.3.4-patch.

SoC: I.MX8MQ and I.MX8MD

Android_release.PNG

Best Regards,

YY

0 件の賞賛
返信

3,089件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

P9.0.0_2.3.2.PNG

This version is only for i.MX8MN and i.MX8QXP, if you are use the i.MX8M series you can try other version.

0 件の賞賛
返信

3,089件の閲覧回数
yyc1975
Contributor III

Hi b45499‌,

We have built our own board with i.MX8MQ and i.MX8MD SoC not EVK.

We use "Android P9.0.0_2.3.2 (Linux 4.14 kernel) Android P9.0.0_2.3.4-patch" as code base of our BSP and added our drivers and modifications.

Is that necessary to use "Correct version BSP" for specific SoC?

For the WOL issue, it should be common issue for any i.MX SoC, isn't it?

Best Regards,

YY

0 件の賞賛
返信

3,089件の閲覧回数
yyc1975
Contributor III

HI b45499‌,

Do you have any idea about the WOL feature on Android platform?

Thanks!

YY

0 件の賞賛
返信