Enable clk02 output on mx8mq

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Enable clk02 output on mx8mq

ソリューションへジャンプ
1,108件の閲覧回数
vanpye00
Contributor II

Hi,

I'm trying to make the imx8mq to output the 24mhz clock signal on its own per this post https://community.nxp.com/t5/i-MX-Processors/enable-CLKO2-for-24MHz-output-clock-on-iMX8MN/m-p/12776... but it's not outputing anything. Is there anything difference should I do for the imx8mq?

0 件の賞賛
返信
1 解決策
1,055件の閲覧回数
vanpye00
Contributor II

I got it to work now.

I'm current using kernel Hardknott. It turns out, for Hardknott, uboot was auto-selecting the customboard legacy dts rather than the customboard dts, which was what I modified. Reconfigured uboot to select the customboard dts resolved the issue.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,090件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

You must check if your GPIO pads are the same ad the MX8MNano, if not change it and should be working.

regards

0 件の賞賛
返信
1,056件の閲覧回数
vanpye00
Contributor II

I got it to work now.

I'm current using kernel Hardknott. It turns out, for Hardknott, uboot was auto-selecting the customboard legacy dts rather than the customboard dts, which was what I modified. Reconfigured uboot to select the customboard dts resolved the issue.

0 件の賞賛
返信