Enable and Use GPIOs in IMX8 Nano ddr4 evk

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Enable and Use GPIOs in IMX8 Nano ddr4 evk

1,366 Views
sharathn25
Contributor I

Hi All,

I am new to NXP IMX8 Processors. I am working on i.MX 8M Nano Evk, I have to enable GPIOs (any two) and simply set it to HIGH/LOW.

In the schematic if we check  the header J1003 we can see the information related to pins that are physically available to use. Here I am not using UART, so the pins UART3_CTS and UART3_RTS are also named GPIO.7 & GPIO.0 respectively, I want them to use it as regular gpios.

j1003.png
So after searching in the internet I found out that we need to add information related to GPIOs in the device tree. Here are some of links for Ref :

https://www.emcraft.com/som/imx-8m/controlling-gpio-in-linux

https://www.digi.com/resources/documentation/digidocs/embedded/dey/2.6/cc8mnano/bsp_r_gpio_8m

https://www.variscite.com/blog/i-mx-device-tree-pinmux-settings/

https://variwiki.com/index.php?title=MX8M_GPIO#Pin_Func_files

https://www.digi.com/resources/documentation/digidocs/embedded/dey/2.6/cc8mnano/bsp_r_pin-multiplexi...

And also if the gpios are enabled, the we can control them using the gpiochip utility.

Following are some of my doubts :

  1. Here https://variwiki.com/index.php?title=MX8M_GPIO#Pin_Func_files it says to set GPIO4_21
    gpioset gpiochip3 21= 1

    But as per schematic it is UART3_CTS (GPIO.7)  & UART_3RTS(GPIO.0),  How can I find which GPIOs are actually available on the header ? and what would be the correct gpiochip and its line number for the GPIOs, where can I find these details?
  2. Is there a standard steps or procedure for enabling  and using the GPIO in i.MX8 evk ?

 

 

0 Kudos
Reply
1 Reply

1,157 Views
k_specka
Contributor II

Abit late but... UART3_CTS and UART3_RTS have no alt mode for gpio when the mini reference is right

0 Kudos
Reply