Enable USB HOST1 on imx6.scm

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Enable USB HOST1 on imx6.scm

559 Views
matthewbach
Contributor II

Does anyone have the variable setting to enable USB HOST1 on the imx6 scm boards? On the eval boards they're not brought out for access, and so the demo images have them disabled as well.

Tags (2)
0 Kudos
2 Replies

409 Views
matthewbach
Contributor II

Where would be appropriate to add similar settings? In a stand alone .dtsi file perhaps? I see the sabre's .dtsi file in the repo, but the ones listed for the scm line are all fixes and android related.

Thanks

0 Kudos

409 Views
igorpadykov
NXP Employee
NXP Employee

Hi Matthew

one can check i.MX6Q Sabre SD schematic spf-27392 and its settings in imx6qdl-sabresd.dtsi

and make in similar way

Schematics (1)
i.MX6_SABRE_SDP_DESIGNFILES
http://www.nxp.com/products/software-and-tools/hardware-development-tools/sabre-development-system/s...

imx6qdl-sabresd.dtsi

linux-imx.git - i.MX Linux Kernel 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos