Enable TPM (infineon slb9670) support in iMX8MM EVK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Enable TPM (infineon slb9670) support in iMX8MM EVK

581件の閲覧回数
gsbalajikrishnan
Contributor II

Hello,

I am using iMX8MM EVK and TPM (Infineon SLB9670).

First of all, checked the spi loop back test in user space of imx8mm board itself by connecting (MOSI pin to MISO pin) and it was working fine.

 How to interface the TPM with imx8mm board?

1. I want to know what the possible ways are to enable tpm2.0(optiga slb9670) with imx8mm board.

2. Does U-Boot and kernel have capability to enable tpm? if it is possible, how can i proceed?

 3. Though I enabled CONFIG_TCG_TPM = y in kernel make menuconfig and included the the content in kernel device tree imx8mm-evk.dts as below, it is not listed in kernel space

&ecspi2 {
    #address-cells = <1>;
    #size-cells = <0>;
    fsl,spi-num-chipselects = <1>;
    pinctrl-names = "default";
    pinctrl-0 = <&pinctrl_ecspi2 &pinctrl_ecspi2_cs>;
    cs-gpios = <&gpio5 13 GPIO_ACTIVE_LOW>;
    status = "okay";

    spidev0: spi@0 {
        reg = <0>;
        compatible = "rohm,dh2228fv";
        spi-max-frequency = <500000>;
    };
    tpm0: slb9670@0 {
        compatible="infineon, slb9670";
        reg = <0>;
        resets = <&tpm_reset>;
        spi-max-frequency = <38000000>;
        interrupt-parent = <&gpio5
        interrupts = <IRQ_TYPE_LEVEL_LOW>;
        status = "okay";
    };
};

is this dts file configuration right?

4. Any other steps need to be followed in order to interface tpm?

kindly let me know your suggestions.

 

Thanks & Regards,

Balajikrishnan.G.S

0 件の賞賛
返信
1 返信

542件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,

For this I believe it would be better to check with the part vendor itself, since the bindings available in the kernel documentation are very simple and pretty much what you already have.

Best regards,
Aldo.

0 件の賞賛
返信