Enable LPSPI2 for iMX8QUADMAX

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Enable LPSPI2 for iMX8QUADMAX

834 次查看
kasandesh
Contributor II

Hello ALL,

What is the procedure to enable SPI2 in iMX8QUADMAX ? 

It is seen from the device tree that lpspi0 is at address 5a000000 and also lpspi3 is at address 5a030000.

lpspi0 creates a flash device and lpspi3 creates a spidev. 

I want to enable the SPI2 device and use it in master mode to connect to a sensor and measure a value.

Any leads on this would be appreciated. 

Best Regards

0 项奖励
回复
1 回复

750 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Sandesh

one can look at explanations provided on

Adding new spi module on IMX8 quad max with Yocto 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复