Enable CSI in IPU_CONF causes board to hang when using Android.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Enable CSI in IPU_CONF causes board to hang when using Android.

跳至解决方案
1,889 次查看
MadsMeisner
Contributor I

i am trying to get a new camera running on MX6Solo. I have the CSI running, and able to capture single-shots using a small console capture program (no gui, no preview). I.e. the route from camera to /dev/video0 seem OK.

I have also enabled the CSI test mode to generate a checker-board. I see this too when I capture with my little console program.

However; If I start the camera app on the phone, now involving Android and possibly preview, I get a kernel stop. A stop with no messages, no dump, nothing, it simply hangs!

The lights go out just after I do "ipu_cm_write(ipu, reg | IPU_CONF_CSI0_EN, IPU_CONF);" (ipu_common.c).

The strange thing is that my small capture program works ok. So I *suspect* it may be in regard with the preview or something else caused by Android.

  • I have tried to log interrupts, and it does not seem I am getting any interrupts after the 'enable' of CSI0, so I don't think it is an interrupt hanging. Maybe it is a bad DMA setup? (however I need a good idea of how to look into that).
  • I have tried hardcoding IPU_CONF to just IPU_CONF_CSI0_EN (to disable as much IPU flow as possible), but it still dies.
  • I have tried skipping the "enable"-line of code, and then the code does NOT crash or hang.

So: In short: I enable CSI0, and the platform stops!

Any ideas are appreciated!

I have logged the following registers just prior to enabling CSI0: They look much the same as for my console capture. Only exception is: IPU_INT_CTRL(10) =      0x777F000F.

IPU_CONF =      0x000007A0

IDMAC_CONF =    0x0000002F

IDMAC_CHA_EN1 =         0x00800001

IDMAC_CHA_EN2 =         0x00000000

IDMAC_CHA_PRI1 =        0x18800001

IDMAC_CHA_PRI2 =        0x00000000

IDMAC_BAND_EN1 =        0x00000000

IDMAC_BAND_EN2 =        0x00000000

IPU_CHA_DB_MODE_SEL0 =  0x00000001

IPU_CHA_DB_MODE_SEL1 =  0x00000000

IPU_CHA_TRB_MODE_SEL0 =         0x00800000

IPU_CHA_TRB_MODE_SEL1 =         0x00000000

DMFC_WR_CHAN =  0x00000090

DMFC_WR_CHAN_DEF =      0x202020F6

DMFC_DP_CHAN =  0x00009694

DMFC_DP_CHAN_DEF =      0x2020F6F6

DMFC_IC_CTRL =  0x00000002

IPU_FS_PROC_FLOW1 =     0x00000000

IPU_FS_PROC_FLOW2 =     0x00000000

IPU_FS_PROC_FLOW3 =     0x00000000

IPU_FS_DISP_FLOW1 =     0x00000000

IPU_VDIC_VDI_FSIZE =    0x00000000

IPU_VDIC_VDI_C =        0x00000000

IPU_IC_CONF =   0x00000000

IPU_INT_CTRL(1) =       0x80000001

IPU_INT_CTRL(2) =       0x00080000

IPU_INT_CTRL(3) =       0x00000000

IPU_INT_CTRL(4) =       0x00000000

IPU_INT_CTRL(5) =       0xBFFEFF2F

IPU_INT_CTRL(6) =       0x001FFF02

IPU_INT_CTRL(7) =       0x00000000

IPU_INT_CTRL(8) =       0x00000000

IPU_INT_CTRL(9) =       0xDC000001

IPU_INT_CTRL(10) =      0x777F000E

IPU_INT_CTRL(11) =      0x00000000

IPU_INT_CTRL(12) =      0x00000000

IPU_INT_CTRL(13) =      0x00000000

IPU_INT_CTRL(14) =      0x00000000

IPU_INT_CTRL(15) =      0x00000000

IPU_SDMA(1) =   0x00000000

IPU_SDMA(2) =   0x00000000

IPU_SDMA(3) =   0x00000000

IPU_SDMA(4) =   0x00000000

IPU_SDMA(5) =   0x00000000

IPU_SDMA(6) =   0x00000000

IPU_SDMA(7) =   0x00000000

IPU_SDMA(8) =   0x00000000

IPU_SDMA(9) =   0x00000000

IPU_SDMA(10) =  0x00000000

IPU_SDMA(11) =  0x00000100

IPU_SDMA(12) =  0x06050803

IPU_SDMA(13) =  0x00000000

IPU_SDMA(14) =  0x00000000

IPU_SDMA(15) =  0x00000000

CSI information for csi0

CSI_CONF =      0x040A8818

CSI_SENS_FRM_SIZE =     0x01DF027F

CSI_ACT_FRM_SIZE =      0x01DF027F

CSI_OUT_FRM_CTRL =      0x00000000

CSI_TST_CTRL =  0x017FFF7F

0 项奖励
回复
1 解答
1,487 次查看
qiang_li-mpu_se
NXP Employee
NXP Employee

You can reference to the Freescale Android BSP document, such as "i.MXAndroidJB4.2.2_1.1.0GAFAQ.html", for "How do I configure rear and front camera" and "how do I configure camera sensor parameters".

If you haven't added the camera sensor correctly, I think it will not get correct buffer for capture, then when enabled CSI, because no correct IDMAC memory address was set, kernel will hang up.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,486 次查看
michaelsadikov
Contributor I

To Mads Meisner & Qiang Li

Tell me please how to read IPU registers (IPU_CONF and others)?

I tried such code

struct ipu_soc *ipu;

ipu = ipu_get_soc(0);
ipu_conf = ipu_cm_read(ipu, IPU_CONF);

It doesn't work

0 项奖励
回复
1,488 次查看
qiang_li-mpu_se
NXP Employee
NXP Employee

You can reference to the Freescale Android BSP document, such as "i.MXAndroidJB4.2.2_1.1.0GAFAQ.html", for "How do I configure rear and front camera" and "how do I configure camera sensor parameters".

If you haven't added the camera sensor correctly, I think it will not get correct buffer for capture, then when enabled CSI, because no correct IDMAC memory address was set, kernel will hang up.

0 项奖励
回复