Electrical Isolation of dedicated signals/pins

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Electrical Isolation of dedicated signals/pins

Jump to solution
1,410 Views
vijayansivamani
Contributor II

Hi,

Can anyone detail how to electrically isolate the dedicated signals/pins in the i.mx6 processor ?

eg., There is short occurred between 5V signal to i.mx6 pin "U3 -LVDS0_TX1_P". Currently this pin U3 is not used in the design but I believe this 5V may damage this pin over long time. So I am planning to electrically isolate this pin from 5V signal internally in the chip(by firmware). Same way there are other dedicated signals have solder short like this. so in general, is it possible to electrically isolate dedicated signals/pins and how it can be done ?

- Vijay

Labels (4)
0 Kudos
Reply
1 Solution
1,323 Views
igorpadykov
NXP Employee
NXP Employee

Hi Vijay

you are right, 5V may damage pin, as it exceed value defined in sect.4.1.1

Absolute Maximum Ratings i.MX6DQ Datasheet

http://www.nxp.com/docs/en/data-sheet/IMX6DQCEC.pdf

Unfortunately there is no way to electrically isolate such pins.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
1,324 Views
igorpadykov
NXP Employee
NXP Employee

Hi Vijay

you are right, 5V may damage pin, as it exceed value defined in sect.4.1.1

Absolute Maximum Ratings i.MX6DQ Datasheet

http://www.nxp.com/docs/en/data-sheet/IMX6DQCEC.pdf

Unfortunately there is no way to electrically isolate such pins.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,323 Views
vijayansivamani
Contributor II

Thanks for the details.