Hi,
I have an issue with my ethernet in uboot. U-Boot 2018.03. In Linux the ethernet works well so I can assume that the hardware is okay.
MyHardware:
i.MX6Q
PHY: Microchip LAN8720A
Phy is connected by RMII as described in Hardware Development Guide for i.MX6 Chapter 12.
Ethernet-Phy (LAN8720) | Prozessor (i.MX6) |
MDIO (12) | ENET_MDIO (V23) |
MDC (13) | ENET_MDC (V20) |
RXD0 (8) | ENET_RXD0 (W21) |
RXD1 (7) | ENET_RXD1 (W22) |
CRS_DV (11) | ENET_CRS_DV (U21) |
TXD0 (17) | ENET_TXD0 (U20) |
TXD1 (18) | ENET_TXD1 (W20) |
TXEN (16) | ENET_TX_EN (V21) |
RST (15) | EIM_BCLK (N22) |
XTAL1/CLKIN (5) | GPIO16 (R2) |
RXER (10) | ENET_RX_ER (W23) |
INT (14) | n.c. |
I configure GPIO16 as clock output (50MHz). I can measure the 50MHz at pin 5 of LAN8720. During the initialisatzion first I configure ENET_RXD0, ENET_RXD1, ENET_CRS_DV and ENET_RX_ER as GPIO and set them all to high to set the mode and address of the PHY. Then I assert a PHY reset and deassert it after 10ms. Then I reconfigure ENET_RXD0, ENET_RXD1, ENET_CRS_DV and ENET_RX_ER.
In uboot I can communicate with the PHY over MII or MDIO. I checked the signals with a logic analyser and it looks okay.
=> mdio list FEC: 1 - SMSC LAN8710/LAN8720 <--> FEC => mii info 1 fec_mdio_read: phy: 01 reg:03 val:0xc0f1 fec_mdio_read: phy: 01 reg:02 val:0x7 fec_mdio_read: phy: 01 reg:00 val:0x3100 fec_mdio_read: phy: 01 reg:05 val:0xcde1 fec_mdio_read: phy: 01 reg:04 val:0x1e1 fec_mdio_read: phy: 01 reg:00 val:0x3100 fec_mdio_read: phy: 01 reg:05 val:0xcde1 fec_mdio_read: phy: 01 reg:04 val:0x1e1 PHY 0x01: OUI = 0x01F0, Model = 0x0F, Rev = 0x01, 100baseT, FDX
But when I want to do a ping-command I always got the following message:
=> ping 192.168.0.155Using FEC device ARP Retry count exceeded; starting again ping failed; host 192.168.0.155 is not alive => pri ipaddr ipaddr=192.168.0.75
After some investigation I add a few debug outputs to the fec_mxc.c to check the pin muxing.
=> ping 192.168.0.155 eth_halt: wait for stop regs eth_halt: done fec_mii_setspeed: mii_speed 0000001a fec_open: fec_open(dev) [fec_open] fec->eth->ecntrl: 0x2188024, reg: 0xf0000102 [fec_open]: use PHYLIB fec_mdio_read: phy: 01 reg:01 val:0x782d fec_mdio_read: phy: 01 reg:01 val:0x782d fec_mdio_read: phy: 01 reg:01 val:0x782d fec_mdio_read: phy: 01 reg:04 val:0x1e1 fec_mdio_read: phy: 01 reg:05 val:0xcde1 [fec_open]: speed = 100 fec_open:Speed=100 [fec_open]: ENET_RDAR 0x1000000 Using FEC device IOMUXC_SW_MUX_CTL_PAD_ENET_MDIO (0x20E01D0): 0x00000001 IOMUXC_SW_MUX_CTL_PAD_ENET_RX_ER (0x20E01D8): 0x00000001 IOMUXC_SW_MUX_CTL_PAD_ENET_CRS_DV (0x20E01DC): 0x00000001 IOMUXC_SW_MUX_CTL_PAD_ENET_RX_DATA1 (0x20E01E0): 0x00000001 IOMUXC_SW_MUX_CTL_PAD_ENET_RX_DATA0 (0x20E01E4): 0x00000001 IOMUXC_SW_MUX_CTL_PAD_ENET_TX_EN (0x20E01E8): 0x00000001 IOMUXC_SW_MUX_CTL_PAD_ENET_TX_DATA1 (0x20E01EC): 0x00000001 IOMUXC_SW_MUX_CTL_PAD_ENET_TX_DATA0 (0x20E01F0): 0x00000001 IOMUXC_SW_MUX_CTL_PAD_ENET_MDC (0x20E01F4): 0x00000001 IOMUXC_SW_MUX_CTL_PAD_EIM_BCLK (0x20E0158): 0x00000005 IOMUXC_SW_MUX_CTL_PAD_GPIO16 (0x20E0248): 0x00000012 IOMUXC_SW_PAD_CTL_PAD_ENET_MDIO (0x20E04E4): 0x0001b0b0 IOMUXC_SW_PAD_CTL_PAD_ENET_RX_ER (0x20E04EC): 0x0001b0b0 IOMUXC_SW_PAD_CTL_PAD_ENET_CRS_DV (0x20E04F0): 0x0001b0b0 IOMUXC_SW_PAD_CTL_PAD_ENET_RX_DATA1 (0x20E04F4): 0x0001b0b0 IOMUXC_SW_PAD_CTL_PAD_ENET_RX_DATA0 (0x20E04F8): 0x0001b0b0 IOMUXC_SW_PAD_CTL_PAD_ENET_TX_EN (0x20E04FC): 0x0001b0b0 IOMUXC_SW_PAD_CTL_PAD_ENET_TX_DATA1 (0x20E0500): 0x0001b0b0 IOMUXC_SW_PAD_CTL_PAD_ENET_TX_DATA0 (0x20E0504): 0x0001b0b0 IOMUXC_SW_PAD_CTL_PAD_ENET_MDC (0x20E0508): 0x0001b0b0 IOMUXC_SW_PAD_CTL_PAD_EIM_BCLK (0x20E046C): 0x000000f1 IOMUXC_SW_PAD_CTL_PAD_GPIO16 (0x20E0618): 0x000000e1 IOMUXC_ENET_MAC0_MDIO_SELECT_INPUT (0x20E0840): 0x00000000 IOMUXC_ENET_MAC0_RX_CLK_SELECT_INPUT (0x20E0844): 0x00000000 IOMUXC_ENET_MAC0_RX_DATA0_SELECT_INPUT (0x20E0848): 0x00000001 IOMUXC_ENET_MAC0_RX_DATA1_SELECT_INPUT (0x20E084C): 0x00000001 IOMUXC_ENET_MAC0_RX_EN_SELECT_INPUT (0x20E0858): 0x00000001 IOMUXC_ENET_REF_CLK_SELECT_INPUT (0x20E083C): 0x00000001 CCM_ANALOG_PLL_ENET (0x20C80E0): 0x80102001 IOMUXC_GPR1 (0x20E0004): 0x48602005 [fec_open]: ENET_TDAR 0x01000000 [fec_send]: timeout TDAR fec_send: status 0x8c00 index 0 ret -22 fec_recv: ievent 0x0 fec_recv: status 0x8000 fec_recv: stop fec_recv: ievent 0x0 fec_recv: status 0x8000 fec_recv: stop fec_recv: ievent 0x0 fec_recv: status 0x8000 ...
I checked the signals on RXD0, RXD1, TXD0 and TXD1 at the PHY while I enter the ping-command. I can see nothing. No edges, nothing. All lines are low.
So is there a missconfiguration of my pin muxing? Is there a clock missing? Currently I am quite at a loss and I lack ideas.
Thanks.
Regards Michael
Hi,
I found the issue. The PHY is connected over RMII and the following config was the mistake:
#define CONFIG_FEC_XCV_TYPE RGMII
It has to be
#define CONFIG_FEC_XCV_TYPE RMII
:smileyconfused: