(Edit) How to change i.MX 8M Quad Evaluation Kit, Win10 iot display resolution?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

(Edit) How to change i.MX 8M Quad Evaluation Kit, Win10 iot display resolution?

1,322 Views
alzip79
Contributor II

Hello. NXP

My Board : i.MX 8M Quad Evaluation Kit

My OS : windows 10 iot

Using MCIMX8M-EVK Image FFU File,

When connected to a monitor that supports 3840x2160 resolution using the native HDMI port, it displays at 1280x720 resolution.

How to change to 3840x2160 Display Resolution?

===========================

I found this document a while ago.

https://www.nxp.com/docs/en/release-note/IMXWNR.pdf 

resol.png

Will this problem be solved soon?

I want to solve this problem in a short time.

Do I need to use a package like i.MX8 or i.MX8M Plus to use 4K resolution?

spec.png

Thank you for your help.

0 Kudos
Reply
2 Replies

1,171 Views
vfilip
NXP Employee
NXP Employee

Hi,

this is SW/BSP limitation. Switch to another 64-bit processor will not resolve this issue for you. I would recommend to follow the steps provided by Jiri Rezler in this thread: https://community.nxp.com/thread/524880

best regards

Vojtech Filip

0 Kudos
Reply

1,171 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Good!

0 Kudos
Reply