Easily build a custom Linux BSP for an i.MX

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Easily build a custom Linux BSP for an i.MX

1,184 次查看
MaciejHalasz
Contributor I

Timesys offers FREE online tools with which you can build a custom BSP for an i.MX processor.

 

http://www.timesys.com/register     (BTW, the tool won Best in Show at FTF)

 

Its actually very easy to use. Using an online web hosted system in only 4 steps driven by a nice wizard you can select the following:

 

1. Linux kernel - based on Freescale LTIB

2. Cross-toolchain - (uClibc or glibc)

3. RFS packages (hundreds of them)

4. Deployment options

 

The entire process of building your BSP happens on Timesys servers and when the build is done, you get an e-mail with a link from where you can download your custom BSP.

You actually get the following:

 

Your custom BSP binaries:

- Linux kernel

- RFS - pre-formatted for deployment with your selected packages (APIs)

 

Matching custom SDK (for application/system development)

- cross-toolchain

- pre-installed header files and libs

 

With the custom BSP/SDK it is easy to try different APIs, build benchmarks, simple apps etc.

Access to the system and ability to build custom BSPs is not time limited.You get access to all the sources as well!

标签 (1)
0 项奖励
回复
1 回复

1,079 次查看
KrishnaPavan
Contributor II

Yeah exactly!

 

But can you tell me the System Boot Flow either in i.MX51X or i.MX53X?

Because I am stuck with the partitions and etc etc............

I was not able to completely understand the concepts................>>>>>>>! 

0 项奖励
回复