Q. Does i.MX issue the SRX command by themself ?
A. Yes.
Q. If 1 is yes, when will it issue the command ?
A. According to the DDR3 JEDEC standard, the issue of the SRX command consists of transitioning the CKE signal from Low to High with the CS# signal staying High. So, the moment of the CKE signal assertion is the moment of issuing the SRX command.
Have a great day,
Artur
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------