EVK Linux not logging in stuck at login prompt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

EVK Linux not logging in stuck at login prompt

1,167 Views
ganeshh
Contributor III

Hi,

I sucessfully booted Linux preloaded SD card on IMX28 EVK. I am getting boot messages at UART Debug port. The booting process stops at the login prompt freescale login: root

When i give the username root and press it remains it wont login or goes to the root prompt ? How to solve this issue? After that am also getting a matchbox error. The login prompt is highlighted in the messages.

BOOT Messages

Welcome to minicom 2.6.2


OPTIONS: I18n


Compiled on Feb 8 2013, 06:27:51.


Port /dev/ttyUSB0, 11:43:16




Press CTRL-A Z for help on special keys




HTLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLFLC


PowerPrep start initialize power...


Battery Voltage = 4.23V


boot from battery. 5v input not detected


LLLCSep 10 201012:30:50


FRAC 0x92925552


Wait for ddr ready 1power 0x00820616


Frac 0x92925552


start change cpu freq


hbus 0x00000003


cpu 0x00010001


start test memory accress


ddr2 0x40000000


finish simple test


LLLLLLLFLCLLJUncompressing Linux...............................................................................................................


Linux version 2.6.31-855-ge067785 (madfsl@ubuntu) (gcc version 4.1.2) #1 Fri Sep 10 09:22:06 MDT 2010


CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177


CPU: VIVT data cache, VIVT instruction cache


Machine: Freescale MX28EVK board


Memory policy: ECC disabled, Data cache writeback


INITRD: 0x40400000+0x00400000 overlaps in-use memory region - disabling initrd


Built 1 zonelists in Zone order, mobility grouping on. Total pages: 32512


Kernel command line: noinitrd console=ttyAM0,115200 root=/dev/mmcblk0p3 rw rootwait ip=none gpmi


PID hash table entries: 512 (order: 9, 2048 bytes)


Dentry cache hash table entries: 16384 (order: 4, 65536 bytes)


Inode-cache hash table entries: 8192 (order: 3, 32768 bytes)


Memory: 128MB = 128MB total


Memory: 124420KB available (4552K code, 658K data, 152K init, 0K highmem)


SLUB: Genslabs=11, HWalign=32, Order=0-3, MinObjects=0, CPUs=1, Nodes=1


Hierarchical RCU implementation.


NR_IRQS:288


Console: colour dummy device 80x30


console [ttyAM0] enabled


Calibrating delay loop... 907.67 BogoMIPS (lpj=4538368)


Security Framework initialized


SELinux: Initializing.


Mount-cache hash table entries: 512


CPU: Testing write buffer coherency: ok


regulator: core version 0.5


NET: Registered protocol family 16


regulator: vddd: 800 <--> 1575 mV fast normal


regulator: vddd_bo: 800 <--> 1575 mV fast normal


regulator: vdda: 1500 <--> 2275 mV fast normal


regulator: vddio: 2880 <--> 3680 mV fast normal


regulator: overall_current: 0 <--> 2147483 mA fast normal


regulator: mxs-duart-1: 0 <--> 2147483 mA fast normal


regulator: mxs-bl-1: 0 <--> 2147483 mA fast normal


regulator: mxs-i2c-1: 0 <--> 2147483 mA fast normal


regulator: mmc_ssp-1: 0 <--> 2147483 mA fast normal


regulator: mmc_ssp-2: 0 <--> 2147483 mA fast normal


regulator: charger-1: 0 <--> 2147483 mA fast normal


regulator: power-test-1: 0 <--> 2147483 mA fast normal


regulator: cpufreq-1: 0 <--> 2147483 mA fast normal


i.MX IRAM pool: 124 KB@0xc8820000


Initializing GPMI pins


usb: DR OTG registered


usb: DR gadget (utmi) registered


audit: cannot initialize inotify handle


bio: create slab <bio-0> at 0


SCSI subsystem initialized


Freescale USB OTG Driver loaded, $Revision: 1.55 $


usbcore: registered new interface driver usbfs


usbcore: registered new interface driver hub


usbcore: registered new device driver usb


NET: Registered protocol family 2


IP route cache hash table entries: 1024 (order: 0, 4096 bytes)


TCP established hash table entries: 4096 (order: 3, 32768 bytes)


TCP bind hash table entries: 4096 (order: 2, 16384 bytes)


TCP: Hash tables configured (established 4096 bind 4096)


TCP reno registered


NET: Registered protocol family 1


Bus freq driver module loaded


mxs_cpu_init: cpufreq init finished


audit: initializing netlink socket (disabled)


type=2000 audit(0.400:1): initialized


VFS: Disk quotas dquot_6.5.2


Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)


JFFS2 version 2.2. (NAND) �© 2001-2006 Red Hat, Inc.


msgmni has been set to 243


alg: No test for stdrng (krng)


cryptodev: driver loaded.


Block layer SCSI generic (bsg) driver version 0.4 loaded (major 253)


io scheduler noop registered


io scheduler anticipatory registered


io scheduler deadline registered


io scheduler cfq registered (default)


Console: switching to colour frame buffer device 100x30


mxs-duart.0: ttyAM0 at MMIO 0x80074000 (irq = 47) is a DebugUART


mxs-auart.0: ttySP0 at MMIO 0x8006a000 (irq = 112) is a mxs-auart.0


Found APPUART 3.1.0


mxs-auart.1: ttySP1 at MMIO 0x8006c000 (irq = 113) is a mxs-auart.1


Found APPUART 3.1.0


mxs-auart.2: ttySP2 at MMIO 0x8006e000 (irq = 114) is a mxs-auart.2


Found APPUART 3.1.0


mxs-auart.3: ttySP3 at MMIO 0x80070000 (irq = 115) is a mxs-auart.3


Found APPUART 3.1.0


brd: module loaded


loop: module loaded


FEC Ethernet Driver


fec_enet_mii_bus: probed


IEEE1588: ptp-timer is unavailable


IEEE1588: ptp-timer is unavailable


i.MX GPMI NFC


NFC: Version 1, 8-chip GPMI and BCH


Boot ROM: Version 1, Single-chip boot area, block mark swapping supported


Scanning for NAND Flash chips...


No NAND device found!!!


gpmi-nfc gpmi-nfc.0: Chip scan failed


ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver


fsl-ehci fsl-ehci: Freescale On-Chip EHCI Host Controller


fsl-ehci fsl-ehci: new USB bus registered, assigned bus number 1


fsl-ehci fsl-ehci: irq 93, io base 0x80080000


fsl-ehci fsl-ehci: USB 2.0 started, EHCI 1.00


usb usb1: configuration #1 chosen from 1 choice


hub 1-0:1.0: USB hub found


hub 1-0:1.0: 1 port detected


fsl-ehci fsl-ehci.0: Freescale On-Chip EHCI Host Controller


fsl-ehci fsl-ehci.0: new USB bus registered, assigned bus number 2


fsl-ehci fsl-ehci.0: irq 92, io base 0x80090000


fsl-ehci fsl-ehci.0: USB 2.0 started, EHCI 1.00


usb usb2: configuration #1 chosen from 1 choice


hub 2-0:1.0: USB hub found


hub 2-0:1.0: 1 port detected


Initializing USB Mass Storage driver...


usbcore: registered new interface driver usb-storage


USB Mass Storage support registered.


ARC USBOTG Device Controller driver (1 August 2005)


mice: PS/2 mouse device common for all mice


input: mxs-kbd as /devices/platform/mxs-kbd.0/input/input0


input: MXS touchscreen as /devices/virtual/input/input1


MXS RTC driver v1.0 hardware v2.3.0


mxs-rtc mxs-rtc.0: rtc core: registered mxs-rtc as rtc0


Linux video capture interface: v2.00


mxs-pxp mxs-pxp.0: initialized


IRQ 6/mxs-battery: IRQF_DISABLED is not guaranteed on shared IRQs


mxs watchdog: initialized, heartbeat 19 sec


mxs-mmc: MXS SSP Controller MMC Interface driver


mxs-mmc mxs-mmc.0: mmc0: MXS SSP MMC DMAIRQ 82 ERRIRQ 96


Registered led device: led-pwm0


Registered led device: led-pwm1


dcp dcp.0: DCP crypto enabled.!


usbcore: registered new interface driver usbhid


usbhid: v2.6:USB HID core driver


Advanced Linux Sound Architecture Driver Version 1.0.20.


regulator: Unable to get requested regulator: VDDIO


regulator: Unable to get requested regulator: VDDA


regulator: Unable to get requested regulator: VDDD


sgtl5000-i2c 0-0014: SGTL5000 revision 17


mmc0: new high speed SDHC card at address aaaa


mmcblk0: mmc0:aaaa SU04G 3.69 GiB


mmcblk0: p1 p2 p3


mxs-spdif mxs-spdif.0: MXS SPDIF Audio Transmitter


No device for codec mxs spdif


No device for DAI mxs spdif


No device for DAI mxs-saif


No device for DAI mxs-spdif


asoc: SGTL5000 <-> mxs-saif mapping ok


Failed to add route LINE_OUT->Ext Spk


asoc: mxs spdif <-> mxs-spdif mapping ok


ASoC: Failed to create codec register debugfs file


Failed to create pop time debugfs file


ALSA device list:


  #0: mxs-evk (SGTL5000)


  #1: mxs-evk (mxs spdif)


TCP cubic registered


NET: Registered protocol family 17


can: controller area network core (rev 20090105 abi 8)


NET: Registered protocol family 29


can: raw protocol (rev 20090105)


RPC: Registered udp transport module.


RPC: Registered tcp transport module.


mxs-rtc mxs-rtc.0: setting system clock to 1970-01-01 01:05:52 UTC (3952)


EXT2-fs warning: mounting unchecked fs, running e2fsck is recommended


VFS: Mounted root (ext2 filesystem) on device 179:3.


Freeing init memory: 152K


USB Host suspended


init started: BusyBox v1.15.0 ()


starting pid 1063, tty '': '/etc/rc.d/rcS'


Mounting /proc and /sys


Starting the hotplug events dispatcher udevd


Synthesizing initial hotplug events


Setting the hostname to freescale


Mounting filesystems


mount: mounting usbfs on /proc/bus/usb failed: No such file or directory


Starting inetd:


Starting the dropbear ssh server:


D-Bus per-session daemon address is: unix:abstract=/tmp/dbus-YmnbAwF4Fa,guid=59d6f45f5561607dd4f186e300000f7d


gtk: creating gdk-pixbuf.loaders


pango: creating module list


starting pid 2196, tty '': '/sbin/getty -L ttyAM0 115200 vt100'


_XSERVTransSocketOpenCOTSServer: Unable to open socket for inet6


_XSERVTransOpen: transport open failed for inet6/freescale:0


_XSERVTransMakeAllCOTSServerListeners: failed to open listener for inet6


(EE) XKB: Couldn't open rules file /usr/share/X11/xkb/rules/base


(EE) XKB: No components provided for device Virtual core keyboard


(EE) XKB: Couldn't open rules file /usr/share/X11/xkb/rules/base


(EE) XKB: No components provided for device (unnamed keyboard)


unrecognised device identifier!




arm-none-linux-gnueabi-gcc (GCC) 4.1.2


root filesystem built on Fri, 10 Sep 2010 12:31:16 -0600


Freescale Semiconductor, Inc.


freescale login: root


matchbox: keyboard does not appear to have a <alt> key.


matchbox: ignoring key shortcut <Alt>n=next




matchbox: keyboard does not appear to have a <alt> key.


matchbox: ignoring key shortcut <Alt>p=prev




matchbox: keyboard does not appear to have a <alt> key.


matchbox: ignoring key shortcut <Alt>c=close




matchbox: keyboard does not appear to have a <alt> key.


matchbox: ignoring key shortcut <Alt>d=desktop




matchbox: keyboard does not appear to have a <alt> key.


matchbox: ignoring key shortcut <Alt>m=!matchbox-remote -mbmenu




matchbox: keyboard does not appear to have a <alt> key.


matchbox: ignoring key shortcut <ctrl><alt>x=!xterm




matchbox: keyboard does not appear to have a <alt> key.


matchbox: ignoring key shortcut <ctrl><alt>r=!rxvt




matchbox: keyboard does not appear to have a <alt> key.


matchbox: ignoring key shortcut <ctrl><alt>e=!!gpe-calender




matchbox: keyboard does not appear to have a <alt> key.


matchbox: ignoring key shortcut <alt>Tab=next




matchbox: keyboard does not appear to have a <alt> key.


matchbox: ignoring key shortcut <alt><shift>Tab=prev




matchbox: keyboard does not appear to have a <alt> key.

matchbox: ignoring key shortcut <alt>space=taskmenu


matchbox: keyboard does not appear to have a <alt> key.

matchbox: ignoring key shortcut <alt>escape=!matchbox-re



matchbox: keyboard does not appear to have a <alt> key.


matchbox: ignoring key shortcut <alt>f4=close




matchbox: Cant find a keycode for keysym 65480


matchbox: ignoring key shortcut f11=fullscreen




Failed to get root pixmap id


matchbox-desktop: loading /usr/lib/matchbox/desktop/tasks.so with args ( None )


matchbox-desktop: loading /usr/lib/matchbox/desktop/dotdesktop.so with args ( None )


user_overides is (nil)


mb-applet-menu-launcher: bonobo-browser.desktop has no icon, png or name


mb-applet-menu-launcher: failed to open /usr/local/share/applications


mb-applet-menu-launcher: failed to open //.applications


mb-desktop-dotdesktop: failed to open /usr/local/share/applications


mb-desktop-dotdesktop: failed to open //.applications


mb-applet-menu-launcher: bonobo-browser.desktop has no icon, png or name


mb-applet-menu-launcher: failed to open /usr/local/share/applications


mb-applet-menu-launcher: failed to open //.applications


mb-applet-menu-launcher: bonobo-browser.desktop has no icon, png or name


mb-applet-menu-launcher: failed to open /usr/local/share/applications


mb-applet-menu-launcher: failed to open //.applications


mb-applet-menu-launcher: bonobo-browser.desktop has no icon, png or name


mb-applet-menu-launcher: failed to open /usr/local/share/applications


mb-applet-menu-launcher: failed to open //.applications



Labels (3)
0 Kudos
Reply
0 Replies