ERROR: nxp-wlan-sdk-git-r0 do_compile: oe_runmake failed and /bin/sh: 1: scripts/mod/modpost: Permi

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ERROR: nxp-wlan-sdk-git-r0 do_compile: oe_runmake failed and /bin/sh: 1: scripts/mod/modpost: Permi

1,218 Views
Gourav
Contributor I

when I am creating image first time for imx8mm board via these command

$source sources/poky/oe-init-build-env

$bitbake phytec-qt5demo-image

it is showing ERROR: nxp-wlan-sdk-git-r0 do_compile: oe_runmake failed , and

/bin/sh: 1: scripts/mod/modpost: Permision denied .

 

Screenshot from 2023-02-15 08-58-00.pngScreenshot from 2023-02-15 08-58-48.png

0 Kudos
Reply
2 Replies

1,204 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @Gourav 

The BSP you use is not maintained by NXP. The BSP we release doesn't have such issue.

0 Kudos
Reply

1,144 Views
Gourav
Contributor I

hey

after changing ubuntu os version this problem solved 

Thanks & Regards ,

Gourav

0 Kudos
Reply