Running: custom board with a NovSOM imx6q
I've read ERR006687, and we feel we should do the hardware mod to work around the erratum in the next board revision.
The description says to mux GPIO6 as ethernet interrupt. My question is what should GPIO6 be connected to? Does it need to be connected to the ethernet phy? Is it already internally connected to the ethernet block in the SoC once muxed?
The EE's are confused.
Thanks,
Joshua
已解决! 转到解答。
Hi Joshua
it can be routed internally using debug signals, as attached
picture shows. For example one can look at
linux-2.6-imx.git - Freescale i.MX Linux Tree
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Joshua
it can be routed internally using debug signals, as attached
picture shows. For example one can look at
linux-2.6-imx.git - Freescale i.MX Linux Tree
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------