ENET_REF_CLK for I.MX6QuadPlus

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ENET_REF_CLK for I.MX6QuadPlus

4,380 次查看
takayuki_ishii
Contributor V

Hello

My customer use i.MX6Quad Plus with PCIe and gigabit-ethernet.

In migration guide(EB810) section 13 Peripherals,

it say that 

• Added a mux to the ENET reference clock to enable clocking direct from ENET PLL. In i.MX 6Dual/6Quad, the reference clock must be sourced from ENET_TX_CLK pad.

But I can not find a difference in Reference Manual.

  1) Is it meen that register setting is not changed, but it not request a external connection between ENET_REF_CLK

       and GPIO_16. is it correct?

The other hand, 

I think that it need not only frequency stability but also duty-cycle,

because RGMII interface use both edge of reference clocks for data and control.

(Reference manual section 23.6.18.2 RGMII interface).

But it is not cleared in datasheet.

I show following community threads,

ENET_REF_CLK (ball V22) duty-cycle requirements on i.MX6 

i.MX6Q ENET.REF_CLK input 

  2) Which is correct requirement of frequency stability, +-50ppm or +-25ppm?

  3) How about duty-cycle requirement. 45% - 55% is correct? or 48% - 52% is requested?

Best regards,

Ishii.

标签 (1)
标记 (1)
0 项奖励
回复
7 回复数

3,742 次查看
takayuki_ishii
Contributor V

Hello, Gusarambula

Thank you for your kindly support.

I will ask it to my customer.

Best regards,

Ishii.

0 项奖励
回复

3,742 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Takayuki Ishii,

(1) You are correct, the external connection required to route the clock from GPIO_16 to ENET_REF_CLK is not required on the i.MX6QP.

(2) (3) I will investigate the frequency stability and duty cycle of the internally generated clock, as this is the configuration that interests you and I cannot find these numbers.

The frequency stability and duty-cycle numbers on the threads were a recommendation but I think they were not the actual numbers of the clock signal generated by the i.MX6.

I’ll let you know as soon as I have more information.

Regards,

0 项奖励
回复

3,742 次查看
b50231katsuhiro
NXP Employee
NXP Employee

Hi gusarambula‌

Could you please follow up?

if you don't have update yet, could you please let us know currently status?

Best Regards

Atsumi

0 项奖励
回复

3,742 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Atsumi,

My apologies.

The answer is to set GPR5 bit 9 to select internal 125mhz clock from ENET PLL.

pastedImage_1.png

However, we do not have the information regarding questions (2) and (3). I'm asking again. I'll let you know when I have more information.

Regards,

0 项奖励
回复

3,742 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Takayuki Ishii,

The recommendation I received was to use good (25-50 ppm) frequency stability and 45%~55% & duty cycle clock source. The frequency stability will affect the performance of the Ethernet module so a better stability will provide better performance up to a point. If you could use around 25ppm would be optimal but 50ppm should also work okay.

I hope this information helps!

Regards,

0 项奖励
回复

3,742 次查看
takayuki_ishii
Contributor V

Hello Gusarambula,

Thank you for your response.

The reason why I am asking about (2)(3) are my customer is connect from clkout of external PHY

to ENET_REF_CLK.

But duty-cycle of external-PHY clkou is moved more than 45% - 55%.

To decide is it OK or not, they are requesting a recommendation value of it.

I am waiting for your additional information.

Best regards,

Ishii.

0 项奖励
回复

3,742 次查看
takayuki_ishii
Contributor V

Hello Gusarambula,

Can I get some additional information about it?

I am looking forward to hearing from you.

Best regards,

Ishii

0 项奖励
回复