EMMC (CMD1) not responding to IMX 6DL

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

EMMC (CMD1) not responding to IMX 6DL

10,801 次查看
dharitrihazarik
Contributor I

Dear expert,

I am using IMX 6Dual Lite processor (MCIMX6U8DVM10AB) and
EMMC 4.51 (MT29PZZZ8D5BKFTF-18 W.95L). The clock(400Khz) is fine from the
processor, but after issuing CMD1 the Present Status Register
(uSDHCx_PRES_STATE) of IMX6DL shows CIHB as 1 which means CMD line of eMMC is
busy and any further commands to the e-MMC will be ignored and it shows
"CMD1 Fail" .I believe, one of the reasons for no response from the
device is incompatible voltage range, but both emmc and the processor are set
to 3.3V.

Your inputs for this situation would be very helpful.

Regards,

Dharitri

标签 (1)
0 项奖励
回复
17 回复数

3,926 次查看
juke-huang
Contributor I

@dharitrihazarik 
Dear Dharitri

I have faced the same issue, response for CMD1 is always 0x00FF8080 which means emmc is in busy status.
Could you help share how you fixed it? Is the reason non-compatibility voltage range?

Many thanks!

jukehuang_0-1698404401001.png

 

 

0 项奖励
回复

5,705 次查看
Muhsin
Contributor I

Hi All, 

This could be a late email, but I am facing the same issues which have been discussed in this post. I am using SAMV70 to interface with eMMC and at the moment I am facing issues when sending the CMD1. When sending this command, I am getting no response and also getting CMD1 fail error message. I am a bit confused about what command number and argument should I send to the eMMC using  CMD1. I tried all of the following arguments, but none worked.  

uint32_t ARG2 = 0x00FF8080;
uint32_t ARG3 = 0xC0FF8080 ;
uint32_t ARG4 = 0x00FF8080;
uint32_t ARG5 = 0x40FF8080; 

I am also reading eMMC specification but could not find any solutions yet. Any help is appreciated, please. 

You can send me an email, if you wanted to help me. darenhaji@gmail.com 

Regards

Muhsin 

0 项奖励
回复

7,760 次查看
georgemakarov
Contributor III

I have faced the same problem on MCU iMX 6ULL.
I use USDHC1 for SD card and USDHC2 for eMMC (Micron MTFC4GACAJCN-1M WT).
I configure the USDHC2 

 

 

&MMC_BASE=0x2194000
Per.Set.Field AD:0x0:0x20C4024 %Long 0x70000 4. ;USDHC2_PODF = 5
Per.Set.Field AD:0x0:0x20C401C %Long 0x20000 1. ;USDHC2_CLK_SEL = 1 (PLL2 PFD0 352MHz)
Data.Set &MMC_BASE+0x04 %LE %Long 0x00010200 ; blk size,cnt
Data.Set &MMC_BASE+0x28 %LE %Long 0x08800020 ; bus width, endian
Data.Set &MMC_BASE+0x2C %LE %Long 0x008E08AF ; 400KHz clk
Data.Set &MMC_BASE+0x34 %LE %Long 0x007F0037 ; BRR,BWR, TCI, CCI interrupt enable
Data.Set &MMC_BASE+0x38 %LE %Long 0x007F0037 ; BRR,BWR, TCI, CCI interrupt enable
Data.Set &MMC_BASE+0x44 %LE %Long 0x00100010 ;read/write fifo threshold level 64bytes

 

 

then send CMD0

 

 

Data.Set &MMC_BASE+0x30 %Long 0xFFFFFFFF ;clear status
Data.Set &MMC_BASE+0x8 %Long 0x0  ;arg
Data.Set &MMC_BASE+0xc %Long 0x0  ;cmd
WAIT 10.ms

 

 

georgemakarov_0-1638786410598.jpeg

 


and then CMD1

 

 

Data.Set &MMC_BASE+0x30 %Long 0xFFFFFFFF ;clear status
Data.Set &MMC_BASE+0x8 %Long 0x0 ;arg
Data.Set &MMC_BASE+0xc %Long 0x01020000 ;cmd1
WAIT 10.ms

 

 

request:

georgemakarov_2-1638786464804.jpeg

response:

georgemakarov_3-1638786479934.jpeg

 

I can see the response on oscilloscope and logic analyzer, but MCU doesn't recognize it and keeps clocking the eMMC.

georgemakarov_9-1638787139259.png

 


The CC bit in INT_STATUS register remains 1.

georgemakarov_4-1638786676612.png

The pins configuration is:

 

 

Data.Set ZSD:0x20E0178 %LE %Long 0x1  ; USDHC2_CLK,  IOMUXC_NAND_RE_B_USDHC2_CLK.alt1
Data.Set ZSD:0x20E017C %LE %Long 0x1  ; USDHC2_CMD,  IOMUXC_NAND_WE_B_USDHC2_CMD.alt1
Data.Set ZSD:0x20E0180 %LE %Long 0x1  ; USDHC2_DAT0, IOMUXC_NAND_DATA00_USDHC2_DATA0.alt1
Data.Set ZSD:0x20E0184 %LE %Long 0x1  ; USDHC2_DAT1, IOMUXC_NAND_DATA01_USDHC2_DATA1.alt1
Data.Set ZSD:0x20E0188 %LE %Long 0x1  ; USDHC2_DAT2, IOMUXC_NAND_DATA02_USDHC2_DATA2.alt1
Data.Set ZSD:0x20E018C %LE %Long 0x1  ; USDHC2_DAT3, IOMUXC_NAND_DATA03_USDHC2_DATA3.alt1
Data.Set ZSD:0x20E01A0 %LE %Long 0x1  ; USDHC2_RESET_B, IOMUXC_NAND_ALE_USDHC2_RESET_B.alt1

Data.Set ZSD:0x20E0404 %LE %Long 0x00010059 ; IOMUXC_SW_PAD_CTL_PAD_NAND_RE_B
Data.Set ZSD:0x20E0408 %LE %Long 0x00017059 ; IOMUXC_SW_PAD_CTL_PAD_NAND_WE_B
Data.Set ZSD:0x20E040C %LE %Long 0x00017059 ; IOMUXC_SW_PAD_CTL_PAD_NAND_DATA00
Data.Set ZSD:0x20E0410 %LE %Long 0x00017059 ; IOMUXC_SW_PAD_CTL_PAD_NAND_DATA01
Data.Set ZSD:0x20E0414 %LE %Long 0x00017059 ; IOMUXC_SW_PAD_CTL_PAD_NAND_DATA02
Data.Set ZSD:0x20E0418 %LE %Long 0x00017059 ; IOMUXC_SW_PAD_CTL_PAD_NAND_DATA03
Data.Set ZSD:0x20E042C %LE %Long 0x00017059 ; IOMUXC_SW_PAD_CTL_PAD_NAND_ALE

 

 


SD Card on USDHC1 works perfectly. By the way, waveform of CMD line of SD Card is a little bit better

georgemakarov_5-1638786960874.jpeg

georgemakarov_6-1638786969854.jpeg

 



The same configuartion and eMMC chip i use in another custom board with MCU MXRT1051 and it MCU receives response properly.

georgemakarov_7-1638787060112.jpeggeorgemakarov_8-1638787081833.jpeg

 

Best regards, George Makarov
0 项奖励
回复

7,737 次查看
georgemakarov
Contributor III

The main reason why MCU ignores the answer from eMMC is besides configuring  SW_MUX_CTL_PAD_* registers i had to configure Daisy registers for these pins as well. 

After I added the following lines to peripherals initialization script MCU recognized the answer from eMMC.

Data.Set ZSD:0x20E0670 %LE %Long 0x2 ; IOMUXC_USDHC2_CLK_SELECT_INPUT.NAND_RE_B_ALT1
Data.Set ZSD:0x20E0678 %LE %Long 0x2 ; IOMUXC_USDHC2_CMD_SELECT_INPUT.NAND_WE_B_ALT1
Data.Set ZSD:0x20E067C %LE %Long 0x2 ; IOMUXC_USDHC2_DATA0_SELECT_INPUT.NAND_DATA00_ALT1
Data.Set ZSD:0x20E0680 %LE %Long 0x2 ; IOMUXC_USDHC2_DATA1_SELECT_INPUT.NAND_DATA01_ALT1
Data.Set ZSD:0x20E0684 %LE %Long 0x1 ; IOMUXC_USDHC2_DATA2_SELECT_INPUT.NAND_DATA02_ALT1
Data.Set ZSD:0x20E0688 %LE %Long 0x2 ; IOMUXC_USDHC2_DATA3_SELECT_INPUT.NAND_DATA03_ALT1


 
And finally I got data from eMMC

CMD1 resp: 0x0C0FF8080
CID register
[127:104] 0x13014E
[103:72] 0x51324A35
[71:40] 0x3441100D
[39:8] 0x0E57558C5
Dual port programming mode enabled
-------(e)MMC FLASH--------
Manufacturer ID: 0x13
Card/BGA: BGA
OEM/Application ID: 0x14E
Product name: Q2J54A
Product revision: 1.0
Serial number: 0xDE57558


 i guess  @dharitrihazarik and others have experienced the same problem. 

Best regards, George Makarov

8,506 次查看
ivan_angelov
Senior Contributor I

I am using different NXP chipset from i.MX processor family but I ran into exactly the same issue - eMMC card replies with 0x00FF8080 to CMD1. In my case the card used to be working for a while but then it went to busy state and nothing helps.

I could not see which reply answered the original question. could you share the reply please?

0 项奖励
回复

7,718 次查看
BiyongSUN
NXP Employee
NXP Employee

1. SD card follows SD Card Association  and emmc follows Jedec. You can see the  in the spec, it mentions it is different spec. Yes, it is similar. that why, linux driver share the sdhci.c as controller driver. and the chip uses the same controller as  silicon design. 

2. It is sequence diagram in the spec. I just see some separate operations here. 

3. I did n't see wave form compare to the spec and point out, it is wrong. 

4. quote georgemakarov's test result, no wrong with the single command and response.  

CMD1 resp: 0x0C0FF8080
CID register
[127:104] 0x13014E
[103:72] 0x51324A35
[71:40] 0x3441100D
[39:8] 0x0E57558C5
Dual port programming mode enabled
-------(e)MMC FLASH--------
Manufacturer ID: 0x13
Card/BGA: BGA
OEM/Application ID: 0x14E
Product name: Q2J54A
Product revision: 1.0
Serial number: 0xDE57558

5. i.MX6 family is deployed as mass production chip with millions. So it has such basic problem. I don't think so. if so, point out the wrong with the spec.  At least, till now, we did get such simple issue with linux driver. 

 

 

 

1png.png

 

2.png

0 项奖励
回复

8,506 次查看
emmanuelkarakas
Contributor I

We are having a similar issue. Has this issue been resolved and if so how ?

0 项奖励
回复

8,506 次查看
mohammad_qasimf
Contributor I

Try sending CMD1 without setting Command CRC check Enable (CCCE) bit in CMD register

0 项奖励
回复

8,506 次查看
dharitrihazarik
Contributor I

Just wanted to add up to above:

Basically, we have checked with same .cmm file on both our board as well as Sabre board. We find that the response is there (observed in oscilloscope on both scenarios), but host in our board is not capturing it to their data registers (CMD Response registers are showing 0x0) whereas Sabre board host is capturing the proper response (CMD response register showing 0x00FF8080).

From Hardware perspective we are running at less than 400Khz and we have checked all the timimg parameters and signal integrity too.

Can you please guide us where and what all things we could check further?

Thanks,

Dharitri

0 项奖励
回复

8,506 次查看
dharitrihazarik
Contributor I

Hi Igor,

We are getting response from eMMC device, so it must not be defective, but the IMX processor is not being able to capture the CMD1 response. We have checked the signals with oscilloscope. They resemble exactly same as produced by the Sabre board emmc till CMD1.

Regards,

Dharitri

0 项奖励
回复

8,506 次查看
dharitrihazarik
Contributor I

Hi Igor,

Many thanks for the suggestion.

Presently, am not booting the eMMC device but trying to communicate with it. The issue that I am facing presently with the communication  between eMMC and IMX processor  is that after issuing CMD1 argument as 0XC0FF8080 or 0x40FF8000 and cmd as 0x1020000, I get a response from emmc as 0x00FF8080. But this response is obtained after decoding the generated waveform and is not detected in the software response(using .cmm file with trace32). Might be the reason for this is the host is not being able to capture the response send by the eMMC.

I  would further like to add that according to JEDEC eMMC standard, the device gives a response of 0X00FF8080 when the device is busy and hence should repeat the cmd1 till the device gets to ready state. I have repeated the cmd1 1000 times, but still at the end I get the result as CMD1 Fail.

From hardware perspective, I have checked all the possible cases regarding timing parameters , rise time, fall time of the signal. They all seem to be fine.

Please provide your valuable suggestions.

Thanks & Regards,

Dharitri

0 项奖励
回复

8,506 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Dharitri

MCIMX6DL-SDP has eMMC and it is working fine with it.

Suggest to check it with this board using NXP uboot.

Best regards

igor

0 项奖励
回复

8,510 次查看
dharitrihazarik
Contributor I

Hi Igor,

Have checked the .cmm file with sabre evaluation board, its working fine. But, in our board we are getting stuck on the initialization phase of emmc. As stated above, the IMX is not being able to capture the response from Card after issuing CMD1.

Regards,

Dharitri

0 项奖励
回复

8,509 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Dharitri

reason may be defective eMMC, so one can change it with SDB board.

Also there may be layout errors on custom board, one can check

signals with oscilloscope.

Best regards

igor

0 项奖励
回复

8,509 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Dharitri

one can check eMMC connections, in particular pull-ups on control lines,

refer to Sabre schematic

i.MX6_SABRE_SDP_DESIGNFILES

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

as for software - check that SION bits are set for i.MX6DL iomux control signals.

One can try to test with uboot, included in latest BSP:

Board Support Packages (29)

L3.14.52_1.1.0_MX6QDLSOLO (REV L3.14.52_1.1.0)

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process... 

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

8,509 次查看
dharitrihazarik
Contributor I

Hi Igor,

Thanks for the reply. I have checked eMMC connections, pull-ups(47K) on control lines(CMD),and have also referred to Sabre schematic. The schematics in our design seems to be fine. From the software perspective, i.MX6DL iomux control signals bits are set as per requirement. Still the CMD1 is failing.

Today when we analysed the waveform that we get on the command line (CMD1), it is observed that there is a proper response for the CMD1 (with argument 0xC0FF8080) from the card. From the waveform, we decoded the response as 0x00FF8080 (the 8080 bytes means the card is a dual voltage range one). As per the JEDEC
standards document it is understood that the card is responding back with  the power up status bit as busy(bit no. 31) and it is in byte access mode(bit no. 30 and 29).

Capture_1.PNG

As per emmc datasheet State diagram, this condition occurs when there is non-compatible voltage range card OR if host cannot use sector mode in cards >2GB.

Capture.PNG

Since we have checked the power levels of emmc and have got the response as 8080; I believe we can rule out
the non-compatibility voltage range and suspect the access mode as the issue here
.

Your suggestions for these would be very helpful.

Thanks & Regards,

Dharitri

0 项奖励
回复

8,509 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Dharitri

Sabre reference board MCIMX6DL-SDP has eMMC and one can test

on it, or solder custom eMMC on it. Use uboot for test.

Best regards

igor

0 项奖励
回复