EMMC启动

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

EMMC启动

1,863 Views
zhaojianbo
Contributor I

我目前在使用mx53,分别使用使用EMMC和SD卡作为启动卡,目前使用SD卡烧写、启动Linux一切正常;使用同样的镜像通过MFG工具进行EMMC烧写时烧写成功,按RESET键时EMMC正常启动,但是下电后,重新上电启动发现UBOOT无法启动,有哪位遇到同样的问题,谢谢!

Labels (2)
0 Kudos
Reply
1 Reply

1,574 Views
DonnyChiu
Contributor II

1. check if the bootmode configuration is correct or not

2. make sure eMMC is power before any other power

3. try and add a serial resistor on the eMMC clock signal, and a capacitor to ground, and adjust the resistor and capacitor value to see if it helps.

     for resistor, try 10ohm ~ 100ohm, capacitor, try 10pF~47pF.

We found something strange with the eMMC clock, need to add some resistor and capacitor to delay or deform the signal before eMMC can bootup correctly some time.