ECSPI3 not working after any activity on GPIO4_IO16

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ECSPI3 not working after any activity on GPIO4_IO16

419件の閲覧回数
lk22
Contributor I

Hi,

Once we drive the GPIO4_IO16 (N19) high or low or as input (high or low), after that SPI NOR Flash does not communicate. We have to reset the board to get the NOR Flash working again.

For NOR flash, we have used following pins:
ESCPI3_SCLK (P24)
ESCPI3_SS0 (P21)
ESCPI3_MISO (P23)
ESCPI3_MOSI (P22)

During this test we have not observed SPI clock and data. In PCB traces from P21 to P24 and N19 are in opposite direction, so there is no doubt of cross-talking.

 

With regards

Lalit

ラベル(2)
タグ(1)
0 件の賞賛
返信
0 返答(返信)