ECSPI3 not working after any activity on GPIO4_IO16

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ECSPI3 not working after any activity on GPIO4_IO16

769 次查看
lk22
Contributor I

Hi,

Once we drive the GPIO4_IO16 (N19) high or low or as input (high or low), after that SPI NOR Flash does not communicate. We have to reset the board to get the NOR Flash working again.

For NOR flash, we have used following pins:
ESCPI3_SCLK (P24)
ESCPI3_SS0 (P21)
ESCPI3_MISO (P23)
ESCPI3_MOSI (P22)

During this test we have not observed SPI clock and data. In PCB traces from P21 to P24 and N19 are in opposite direction, so there is no doubt of cross-talking.

 

With regards

Lalit

标签 (2)
标记 (1)
0 项奖励
回复
0 回复数