Dear all,
I'm trying to activate cspi1 on gpio 4-6 and 4-7 for sabre sd.
So i had in my board file :
| MX6Q_PAD_KEY_COL0__ECSPI1_SCLK, | |
| MX6Q_PAD_KEY_ROW0__ECSPI1_MOSI, | |
| MX6Q_PAD_KEY_ROW1__GPIO_4_9, |
But after the boot my line MOSI is high, if i understand well it should be low. In addition to this when i ask for a spi_write i dont see any signal on either SCLK or MOSI.
The only thing working is the Chip select.
I have to precise that i initialize also CSPI3 in my code but i dont have a way to test it.
Please help me to understand how do i have to setup my spi1 lines.
After some investigation, i discovered that SPI was workin but in opposition to all SPI chronograms i saw, MOSI line is up by default.
#define SPI_IMX2_3_CONFIG_DATA_CTL ( 0xf << 16)
We can add this to the driver spi_imx in order to put MOSI line to low by default.
Hope it can help someone
I am not an expert on this area, but every time I need to check some register configuration, I usually look at the iMX6 Platform SDK. There is a test for validating eCSP in Master mode. Look for it on the freescale.com site.