ECSPI clk polarity issue IMX6dq

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ECSPI clk polarity issue IMX6dq

2,079 Views
khaledali
Contributor III

Hi all, 
I'm facing an awkward problem with ecspi. I tried to change the polarity of the clk and read the configuration register to be sure. 
and i found that the polarity bit in my  channel has been changed but without any effect.

are there any other bits to check?

Tags (3)
0 Kudos
Reply
3 Replies

1,959 Views
khaledali
Contributor III

thanks igor 
i have just figure out the problem in the configuration 
in the SCLK_CTL bits in the configuration register 

1,959 Views
igorpadykov
NXP Employee
NXP Employee

Hi Khaled

please try to reset block and follow sect.21.5 Initialization

i.MX6DQ Reference Manual (rev.0  2/2016)
http://cache.nxp.com/files/soft_dev_tools/doc/support_info/iMX6DQPRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,959 Views
khaledali
Contributor III

Thanks igor for you answer.
I tried to do the same initialization but if i tried to change the polarity the bit inside the
configuration register changed but the the idle state of the clk still low.

so this is my configurations I'm using the SDK driver after little modifications please see the configuration function 
I'm using ecspi instance 2 
with param variable :
.channel = 1.
.mode = 1
.ss_pol = 0
.sclk_pol = 1
.sclk_pha = 1
.pre_div = 14
.post_div = 2

The  configuration function :

int ecspi_configure(dev_ecspi_e instance, const param_ecspi_t * param)
{
// Reset eCSPI controller
HW_ECSPI_CONREG(instance).B.EN = 0;

// Enable the clock*
clock_gating_config(REGS_ECSPI_BASE(instance), CLOCK_ON);

//Enable the ECSPI*
HW_ECSPI_CONREG(instance).B.EN = 1;

// Configure IO signals
ecspi_iomux_config(instance);

// Setup chip select
HW_ECSPI_CONREG(instance).B.CHANNEL_SELECT = param->channel;

// Setup mode
uint32_t channelMask = 1 << param->channel;
uint32_t value = HW_ECSPI_CONREG(instance).B.CHANNEL_MODE;
BW_ECSPI_CONREG_CHANNEL_MODE(instance, param->mode ? (value | channelMask) : (value & ~channelMask));

// Setup pre & post clock divider
HW_ECSPI_CONREG(instance).B.PRE_DIVIDER = (param->pre_div == 0) ? 0 : (param->pre_div - 1);
HW_ECSPI_CONREG(instance).B.POST_DIVIDER = param->post_div;

// Setup SCLK_PHA, SCLK_POL, SS_POL
value = HW_ECSPI_CONFIGREG(instance).B.SCLK_PHA;
HW_ECSPI_CONFIGREG(instance).B.SCLK_PHA = param->sclk_pha ? (value | channelMask) : (value & ~channelMask);

value = HW_ECSPI_CONFIGREG(instance).B.SCLK_POL;
HW_ECSPI_CONFIGREG(instance).B.SCLK_POL = param->sclk_pol ? (value | channelMask) : (value & ~channelMask);

value = HW_ECSPI_CONFIGREG(instance).B.SS_POL;
HW_ECSPI_CONFIGREG(instance).B.SS_POL = param->ss_pol ? (value | channelMask) : (value & ~channelMask);

HW_ECSPI_CONFIGREG(instance).B.SS_CTL |= channelMask;

return SUCCESS;
}

0 Kudos
Reply