ECSPI Read and Write Timings

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ECSPI Read and Write Timings

ソリューションへジャンプ
2,087件の閲覧回数
philippechapet
Contributor I

Dear,

On this document, en page 77:

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6SDLAEC.pdf?fasp=1

The tclk timings are 43ns for Read and 15ns for Write.

However the ECSPI is a shift registry. So for each clk, there is a read and a write.

So what is the difference between "ECSPIx_SCLK Cycle Time–Read" and "ECSPIx_SCLK Cycle Time–Write" ?

Best regards

Philippe

ラベル(6)
0 件の賞賛
返信
1 解決策
1,883件の閲覧回数
Yuri
NXP Employee
NXP Employee

   The hardware specs of i.MX6 Datasheet(s) regarding eCSPI timings are results

of tests. Requirements for reliable read are more strict than for writing. One of SPI
ideas is simultaneous read and write ops (implemented as a common shift register),

but there are devices that support SPI interface, but do not need both read and write
ops.  To say roughly we can use "slow" ADC and "fast" DAC.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,884件の閲覧回数
Yuri
NXP Employee
NXP Employee

   The hardware specs of i.MX6 Datasheet(s) regarding eCSPI timings are results

of tests. Requirements for reliable read are more strict than for writing. One of SPI
ideas is simultaneous read and write ops (implemented as a common shift register),

but there are devices that support SPI interface, but do not need both read and write
ops.  To say roughly we can use "slow" ADC and "fast" DAC.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信