Has anybody tried H27UBG8T2BTR/CTR on linux for iMX28?
I'm trying to add some new NAND flash support to the kernel for iMX28 from L2.6.35_10.12.01_SDK. But it seems not to work. I'm using UBIFS as the filesystem.
For the NAND H27UBG8T2CTR, here is the information printed by kernel while booting. I added some items in the array in nand_device_info.c, and modified code to support the page geometry of 8192+640.
-----------------------------
NAND Flash Device Information
-----------------------------
Manufacturer : Hynix (0xad)
Device Code : 0xd7
Cell Technology : MLC
Chip Size : 4 GiB
Pages per Block : 256
Page Geometry : 8192+640
ECC Strength : 20 bits
ECC Size : 1024 B
Data Setup Time : 15 ns
Data Hold Time : 10 ns
Address Setup Time: 20 ns
GPMI Sample Delay : 6 ns
tREA : 20 ns
tRLOH : 5 ns
tRHOH : 15 ns
Description : H27UBG8T2BTR (4GB, 1CE); H27UBG8T2CTR (4GB, 1CE)
-----------------
Physical Geometry
-----------------
Chip Count : 1
Page Data Size in Bytes: 8192 (0x2000)
Page OOB Size in Bytes : 640
Block Size in Bytes : 2097152 (0x200000)
Block Size in Pages : 256 (0x100)
Chip Size in Bytes : 4294967296 (0x100000000)
Chip Size in Pages : 524288 (0x80000)
Chip Size in Blocks : 2048 (0x800)
Medium Size in Bytes : 4294967296 (0x100000000)
------------
NFC Geometry
------------
ECC Algorithm : BCH
ECC Strength : 20
Page Size in Bytes : 8832
Metadata Size in Bytes : 10
ECC Chunk Size in Bytes: 512
ECC Chunk Count : 16
Payload Size in Bytes : 8192
Auxiliary Size in Bytes: 28
Auxiliary Status Offset: 12
Block Mark Byte Offset : 7694
Block Mark Bit Offset : 4
When I created a new ubi volume on /dev/mtd1 and mounted it at the first time, evrything is ok. And after I umounted it and then mount it again, I got some io error. The error -74 is EBADMSG which means ECC failed. See the following logs:
$ ubiformat /dev/mtd1
ubiformat: mtd1 (nand), size 2013265920 bytes (1.9 GiB), 960 eraseblocks of 2097
152 bytes (2.0 MiB), min. I/O size 8192 bytes
libscan: scanning eraseblock 959 -- 100 % complete
ubiformat: 959 eraseblocks are supposedly empty
ubiformat: 1 bad eraseblocks found, numbers: 517
ubiformat: formatting eraseblock 959 -- 100 % complete
$
$ ubiattach /dev/ubi_ctrl -m 1
UBI: attaching mtd1 to ubi0
UBI: physical eraseblock size: 2097152 bytes (2048 KiB)
UBI: logical eraseblock size: 2080768 bytes
UBI: smallest flash I/O unit: 8192
UBI: VID header offset: 8192 (aligned 8192)
UBI: data offset: 16384
UBI: attached mtd1 to ubi0
UBI: MTD device name: "gpmi-nfc-general-use"
UBI: MTD device size: 1920 MiB
UBI: number of good PEBs: 959
UBI: number of bad PEBs: 1
UBI: max. allowed volumes: 128
UBI: wear-leveling threshold: 4096
UBI: number of internal volumes: 1
UBI: number of user volumes: 0
UBI: available PEBs: 946
UBI: total number of reserved PEBs: 13
UBI: number of PEBs reserved for bad PEB handling: 9
UBI: max/mean erase counter: 0/0
UBI: image sequence number: 440121938
UBI: background thread "ubi_bgt0d" started, PID 2832
UBI device number 0, total 959 LEBs (1995456512 bytes, 1.9 GiB), available 946 L
EBs (1968406528 bytes, 1.8 GiB), LEB size 2080768 bytes (2.0 MiB)
$
$ ubimkvol /dev/ubi0 -N rootfs -s 1024MiB
ubiblka: unknown partition table
Volume ID 0, size 517 LEBs (1075757056 bytes, 1.0 GiB), LEB size 2080768 bytes (
2.0 MiB), dynamic, name "rootfs", alignment 1
$
$ mount -t ubifs ubi0:rootfs /mnt/pp/
UBIFS: default file-system created
UBIFS: mounted UBI device 0, volume 0, name "rootfs"
UBIFS: file system size: 1057030144 bytes (1032256 KiB, 1008 MiB, 508 LEBs)
UBIFS: journal size: 33292288 bytes (32512 KiB, 31 MiB, 16 LEBs)
UBIFS: media format: w4/r0 (latest is w4/r0)
UBIFS: default compressor: lzo
UBIFS: reserved for root: 4952683 bytes (4836 KiB)
$
$ umount /mnt/pp/
UBIFS: un-mount UBI device 0, volume 0
$
$ mount -t ubifs ubi0:rootfs /mnt/pp/
UBI error: ubi_io_read: error -74 while reading 2080768 bytes from PEB 513:16384
, read 2080768 bytes
UBI error: ubi_io_read: error -74 while reading 2080768 bytes from PEB 513:16384
, read 2080768 bytes
UBI error: ubi_io_read: error -74 while reading 2080768 bytes from PEB 514:16384
, read 2080768 bytes
UBIFS: recovered master node from LEB 1
UBIFS: mounted UBI device 0, volume 0, name "rootfs"
UBIFS: file system size: 1057030144 bytes (1032256 KiB, 1008 MiB, 508 LEBs)
UBIFS: journal size: 33292288 bytes (32512 KiB, 31 MiB, 16 LEBs)
UBIFS: media format: w4/r0 (latest is w4/r0)
UBIFS: default compressor: lzo
UBIFS: reserved for root: 4952683 bytes (4836 KiB)
$
$ umount /mnt/pp/
UBIFS: un-mount UBI device 0, volume 0
But if I run nandtest with /dev/mtd1, it could pass it without errors. I tried ext3 filesystem on /dev/mtdblock1, it also failed with some I/O error when I was writing a lot of files on it.
And I tried another NAND H27UBG8T2BTR. When I was trying to mount the UBI partition the second time, it told me some PEB is scrubbed and run torture test for it.
So could iMX28 support such kind of NAND? Or is anything I did wrong? Thanks!
The datasheet could be found in the attachment.