EC25E EVB bring up issue in i.MX8

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

EC25E EVB bring up issue in i.MX8

633 Views
vsuneja63
Contributor III

Hi,

Thanks!

I am trying to bring up EC25E EVB in i.MX8MQ EVK. When i am connecting EC25 via USB to i.mx8 then its not detecting board. I have enabled all the kernel configurations given in EC25 driver pdf. Only difference i found is the "option.c" file is not there in my kernel, at the same path i found "option.mod.c" file. Same for other source files also like "usb_wwan.mod.c". I am using kernel 5.4.114. when i compare the source file given in Quectel EC25 sources(option.c) & in my kernel(option.mod.c) are completely different. I have added networkmanager & modemmanager also in my image. I am clueless here what needs to be done to get the driver up. Attaching both the source files for reference.

As it is blocking for me, any input on this will be highly appreciated.

  

Labels (1)
0 Kudos
1 Reply

627 Views
igorpadykov
NXP Employee
NXP Employee

Hi Vipul

 

one can look at below link

https://boundarydevices.com/ec25-modem-android-support-for-i-mx-platforms/

 

Best regards
igor

0 Kudos