Dual video output on ubuntu in imx6q

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Dual video output on ubuntu in imx6q

1,409 Views
mrleo
Contributor IV

Hi all,

Lvds and hdmi dual display on ubuntu in our customer board(i.MX6Q SDB),when lvds and hdmi all set 1920x1080p60, dual video output can not be ok,if lvds output video,the hdmi video can not output! if lvds set 1920x1080p60,and hdmi set 1280x720p60,dual video out will be ok! How can I dual video output be ok if lvds and hdmi all set 1920x1080p60?

Thanks,

Leo

Labels (4)
0 Kudos
Reply
2 Replies

1,005 Views
igorpadykov
NXP Employee
NXP Employee

Hi mrleo

dual 1920x1080p60 video is not supported by i.MX6 hardware,

check below

https://community.freescale.com/docs/DOC-93788

Best regards

chip

0 Kudos
Reply

1,005 Views
Yuri
NXP Employee
NXP Employee

According to the thread, linked below :

"we donot have the multiple display feature supported yet in X11 on

i.MX6. Other option is to use wayland-weston".

"i.mx6q Enable Dual Display of Ubuntu"

https://community.freescale.com/message/392848#392848

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply