Dual screens Single DRM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Dual screens Single DRM

跳至解决方案
1,060 次查看
sebastian-verge
Contributor I

I have been following the Multi-display - Redirecting the output - one DRM interface document.

I can get each app working individually. For some reason I cannot get both applications to start at the same time.

I started by getting the wayland app-ids:

 

torizon@verdin-imx8mp-15207741:~$ docker compose run --rm -e WAYLAND_DEBUG=1 infotainment 2>&1 | grep set_app_id
[3625339.789]  -> xdg_toplevel@24.set_app_id("StarOSApp")
^C
torizon@verdin-imx8mp-15207741:~$ docker compose run --rm -e WAYLAND_DEBUG=1 dash 2>&1 | grep set_app_id
[3645913.156]  -> xdg_toplevel@24.set_app_id("StarDashApp")

 

I added these values to my weston.ini:

 

torizon@verdin-imx8mp-15207741:~$ cat weston.ini 
[core]
idle-time=0
require-input=false
xwayland=true
modules=screen-share.so
shell=kiosk-shell.so
#require-outputs=all-found

[shell]
panel-position=top
locking=false
allow-zap=true
num-workspaces=1

[output]
name=HDMI-A-2
mode=preferred
app-ids=StarDashApp

[output]
name=HDMI-A-1
mode=preferred
app-ids=StarOSApp

 

The docker compose file I am using is as close to https://github.com/toradex/torizon-samples/blob/bookworm/multi-display/single-drm-interface/docker-c... as I can manage. I can post it if that helps?

When I try to start the second container I get the following:

 

torizon@verdin-imx8mp-15207741:~$ docker stats --no-stream
CONTAINER ID   NAME                  CPU %     MEM USAGE / LIMIT     MEM %     NET I/O       BLOCK I/O        PIDS
3a0b29ca1608   live-infotainment-1   44.68%    111MiB / 7.754GiB     1.40%     3.43kB / 0B   0B / 61.4kB      9
7e96d7a3546c   live-weston-1         16.12%    18.26MiB / 7.754GiB   0.23%     0B / 0B       32.8kB / 307kB   11
torizon@verdin-imx8mp-15207741:~$ docker compose up dash --no-deps
[+] Running 1/1
 ✔ dash Pulled    0.7s
[+] Running 1/0
 ✔ Container live-dash-1  Created    0.0s
Attaching to live-dash-1
live-dash-1  | Loaded language: "en"
live-dash-1  | Font "Inter-Bold.ttf" loaded
live-dash-1  | Font "Inter-Medium.ttf" loaded
live-dash-1  | Font "Inter-Regular.ttf" loaded
live-dash-1  | Font "Inter-SemiBold.ttf" loaded
live-dash-1 exited with code 139

 

I am really hoping you can point me to where I can even start to work out what is going on!

0 项奖励
回复
1 解答
865 次查看
sebastian-verge
Contributor I

I asked over in the Toradex community: https://community.toradex.com/t/25126

You can see how our issues were resolved there.

 

Thank you!

在原帖中查看解决方案

0 项奖励
回复
3 回复数
866 次查看
sebastian-verge
Contributor I

I asked over in the Toradex community: https://community.toradex.com/t/25126

You can see how our issues were resolved there.

 

Thank you!

0 项奖励
回复
883 次查看
MaazPatni
Contributor II

Don't Know, @toradex  or or their develop partners like Silicon Signals can help i have seen there are various development done by them on this board.
Here's the reference: https://youtu.be/bUD6gcjBe2o?si=hZgK9GD6scdONsRG

Toradex page: https://www.toradex.com/support/partner-network/services/400014/silicon-signals-pvt-ltd

 

0 项奖励
回复
1,023 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Do not know if it possible in your board, maybe Someone at @toradex can help.

regards