Dual camera support for i.MX8M EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Dual camera support for i.MX8M EVK

1,736 Views
deexithamba
Contributor III

Hello,

I was working on i.MX8M EVK with Android platform and came to know that both the ov5640_mipi cameras are controlled by i2c1 with same i2c address. Is there any way i can use both the cameras simultaneously?? If so, can you please help in getting both the cameras up on the EVK!!

Regards,

Deexith V

0 Kudos
3 Replies

1,293 Views
igorpadykov
NXP Employee
NXP Employee

Hi Deexith

rev.B4/B5 board has different i2c ports for two cameras, please check latest schematic

Design Files for the i.MX 8M Evaluation Kit (EVK)

i.MX 8M Evaluation Kit|NXP 

fsl-imx8mq-evk.dts\freescale\dts\boot\arm64\arch - linux-imx - i.MX Linux kernel 

If this custom board one can design it using different i.MX8M i2c buses.

Test for 2 camera streams:

root@imx8mqevk:~# gst-launch-1.0 glvideomixer name=m sink_0::ypos=0 sink_0::xpos=0 sink_1::ypos=160 sink_1::xpos=0 ! glimagesink  v4l2src device=/dev/video0 ! videoscale ! video/x-raw,width=160,height=160 ! m.  v4l2src device=/dev/video1 ! videoscale ! video/x-raw,width=160,height=160 ! m.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

1,293 Views
deexithamba
Contributor III

Hello igorpadykov,

We are working on B3 revision board.

Regards,

Deexith

0 Kudos

1,293 Views
igorpadykov
NXP Employee
NXP Employee

Hi Deexith

suggest to obtain latest board revision.

Best regards
igor

0 Kudos