Dual camera & dual display working on MYIR's MYD-JX8MX Dev Board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Dual camera & dual display working on MYIR's MYD-JX8MX Dev Board

1,290 Views
kiddy_xu
Contributor III

MYD-JX8MX development board (http://www.myirtech.com/list.asp?id=608) based on NXP i.MX8M quad processors provides powerful multi-media functions including dual displays, dual cameras, high-quality audio, etc. The target applications scale from consumer home audio to industrial building automation and mobile computers requiring high-performance and low-power processors.

Highlights:

- MYC-JX8MX CPU Module as Controller Board

- NXP i.MX 8M Quad Application Processor

- 1GB / 2GB LPDDR4, 8GB eMMC Flash, 256Mbit QSPI Flash

- RS232, 4 x USB 3.0 Host, 1 x USB 3.0 Host/Device, PCIe 3.0 (x4) NVMe SSD Interface, TF Card Slot

- Supports Gigabit Ethernet, WiFi/BT and 4G LTE

- 2 x MIPI-CSI, HDMI, 2 x LVDS, MIPI-DSI, Audio Input/Output

Labels (1)
Tags (1)
0 Kudos
3 Replies

1,108 Views
LinhNguyen
Contributor III

Hi kiddy.xu@myirtech.com‌,
Where can I find the code for this board? I have just bought this board, but can't find its code yet.

0 Kudos

1,107 Views
kiddy_xu
Contributor III

Hi Linh. Please send email to support@myirtech.com.

0 Kudos

1,108 Views
art
NXP Employee
NXP Employee

Thank you for sharing the information.

Best Regards,

Artur

0 Kudos